STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why would ADC show 0.8v while nothing is connected to pin?

Posted on September 23, 2012 at 07:38I have stmf4discovery board with an LCD screen connected via FCMC. I've taken the ADC3_DMA StdPeriph example and adopted it to use PC1 pin since my board does not have PF7 (I hope it does not). So, if I apply 3v ...

arro239 by Senior
  • 3822 Views
  • 8 replies
  • 0 kudos

STM32F103 ext SRAM to SPI failure

Posted on January 26, 2013 at 20:30Hello to all, I have a design where cpu has to transfer blocks of data to a uSD card working in SPI2 mode. My routine is : static void SPIblockTxDMA(uint8_t *SD_Buffer_Tx,uint16_t Len) {   SPI_Cmd(SPI_SDMEM, DISABL...

abrous3d by Associate II
  • 702 Views
  • 0 replies
  • 0 kudos

STM32 M0/M3 simulation

Posted on January 11, 2013 at 10:40I tried to revive an older thread, but that seems not possible if it dates back before the last database meltdown ... Is there any simulation of STM32 MCUs available, specifically the F0 and F1 ? And I don't mean t...

pre set values in sram

Posted on January 26, 2013 at 14:13I want to add some features to my program where it remembers some settings, i want to do this by storing the values in the sram.But when i upload the firmware to the stm32 i need these values to be preset to a cert...

russdx by Associate II
  • 1233 Views
  • 1 replies
  • 0 kudos

F4 DMA to SDIO NDTR Problem

Posted on January 26, 2013 at 01:26Somehow I can not reply to https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy%2est%2ecom%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fDMA%20to...

picguy2 by Associate II
  • 678 Views
  • 0 replies
  • 0 kudos

STM32F051 EEPRom emulation (AN4061)

Posted on January 25, 2013 at 17:12Hi All, According to the apps note AN4061, a page erase should only occur when one page is full. For instance, after the first run and the memory is formatted, page0 is marked as VALID_PAGE, and page1 is marked as...

Re-program Product

Posted on January 25, 2013 at 06:39Dear All, I bought any product that contained STM32F103C8T6 48-pin mcu. I try to re-program it with my own hex file using Flash Loader Demonstrator and it can be wrote and verified correctly but the application can...

zamzoni by Associate II
  • 2283 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.