2019-09-30 12:23 PM
Hello,
On my custom design board, I use external 12 bit ADC (ADS7886) and STM32F767VI. I try to get digitized ADC values with SPI interface. I set the SPI as Receive only master than prescaler as 8; baudrate as 13.5 Mbits/s; polarity as 1; phase as 1; data size as 16 bits; MSB.
My C code in Keil is
uint16_t ADC_Buf;
if(Rx_flag)
{
HAL_GPIO_WritePin(ADC_CS_GPIO_Port, ADC_CS_Pin, GPIO_PIN_RESET);
HAL_SPI_Receive(&hspi4, (uint8_t*)&ADC_Buf,2,100);
volt = (float)(ADC_Buf * 5 / pow(2,12)); //
HAL_GPIO_WritePin(ADC_CS_GPIO_Port, ADC_CS_Pin, GPIO_PIN_SET);
Rx_flag = 0;
}
I enabled SPI global interrupt. Then I set a timer. Timer frequency is at least 10 times bigger frequency than the input signal frequency. Every each interrupt of the timer, a flag is active then transmission happen. But I didn't plot in STM Studio and observe in debugger mode successfully yet. For example, now my input signal frequency is 1.96kHZ and I set the timer as 20kHz.
Do you have any idea to solve this problem?
Thank you,
2019-09-30 1:50 PM
Maybe you want to take one step at a time.
Starting with basic blinky, then with PWM, determining proper timing, etc.
JW
2019-09-30 10:48 PM
If in your mind spi master means you are in control of the sck clock generation, then only spi full duplex bi directional 4 wire shall meet expectations.
2019-10-02 1:21 PM
2019-10-02 3:04 PM
Just don't use the Receive-only mode. It immediately starts to generate clocks as soon as you enable it, and it won't stop until you disable it.
Use normal duplex mode as KIC/HD said above; you don't need to bring out MOSI to a pin.
JW
2019-10-03 1:26 PM
I modified SPI mode as full duplex master. Then I make it pull down of MOSI pin. I correctly read a step signal such as 2.3V fed signal to the ADC. But when I feed biphasic signal. I can only read maximum value of the signal. Then I modified my code a little bit such as
uint8_t ADC_Buf[2];
float testdata_in[16];
uint8_t i=0;
uint16_t ADC_Buf_Val = 0;
uint16_t Sample;
float volt = 0;
void ADC_Conversion_of_Voltage_Transients()
{
HAL_GPIO_WritePin(ADC_CS_GPIO_Port, ADC_CS_Pin, GPIO_PIN_RESET);
HAL_SPI_Receive(&hspi4,ADC_Buf,2,100);
HAL_GPIO_WritePin(ADC_CS_GPIO_Port, ADC_CS_Pin, GPIO_PIN_SET);
Sample = (((uint16_t) ADC_Buf[1]) << 8 | ADC_Buf[0]);
//Sample = 0x0 << 12 | ADC_Buf;
volt = (float)(Sample * (5.0 / 4096.0)); //
testdata_in[i++]=volt;
i %= 16;
}
/* SPI4 init function */
static void MX_SPI4_Init(void)
{
/* SPI4 parameter configuration*/
hspi4.Instance = SPI4;
hspi4.Init.Mode = SPI_MODE_MASTER;
hspi4.Init.Direction = SPI_DIRECTION_2LINES;
hspi4.Init.DataSize = SPI_DATASIZE_16BIT;
hspi4.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi4.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi4.Init.NSS = SPI_NSS_SOFT;
hspi4.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;
hspi4.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi4.Init.TIMode = SPI_TIMODE_DISABLE;
hspi4.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi4.Init.CRCPolynomial = 7;
hspi4.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi4.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi4) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.