2023-12-13 5:33 PM
STM32F051C8T6产品,想用来和多摩川的编码器产品通讯,发送数据0x02,多摩川编码器发送6个字节返回。但用6个字节的中断得不到数据,用6个字节读取也无法得到数据。中断只能收到一个字节,02。有指导问题出在哪里了?
2023-12-14 9:25 AM
TRANSLATION:
STM32 RS485 Communication - Can I receive data at 2.5Mbps baud rate?
STM32F051C8T6 product, I want to use it to communicate with Tamagawa's encoder product, send data 0x02, Tamagawa encoder sends 6 bytes back. But I can't get data with 6 bytes interrupt, and I can't get data with 6 bytes read. The interrupt can only receive a byte, 02. there is a guide to where the problem is?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.