STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to do ADC -> DMA in double buffer mode configuration

Hi All,I am trying to implement a code on STM32H723 Nucleo-144 where the ADC uses DMA configured in double buffer mode. I cant find any examples on how to do it. I have tried to analyze the ADC to DMA in circular mode code, but I struggle to convert ...

elso by Senior
  • 6374 Views
  • 9 replies
  • 1 kudos

Resolved! STM32f103c8t6 how to comfigure TIM3 for a period of 5ms

Hi community,I am trying to port a project from old library maple leaf or older built for Arduino to to STM32cubeIDEthis function I couldn't find any ref to it, my guess it that is sets the period to 5ms Timer3.setPeriod(1000 / 200); browsing some th...

Keita by Associate II
  • 6375 Views
  • 8 replies
  • 1 kudos

Resolved! How to I disable the USB on the STM32L4

Hi I am using the USB CDC on a STM32L433 with the command MX_USB_DEVICE_Init(); to communicate through the USB. In my app, I go into standby mode (by using the HAL_PWR_EnterSTANDBYMode()) command. How do I disable the USB before entering standby?  I ...

Can USB CDC_Receive_FS Callback be called more than once

Hello,I've enabled a USB virtual com port on an STM32F373 successfully.  The CDC_Receive_FS function in usbd_cdc_if.c gets called when data is received.  I never expect to never receive a 'packet' greater than 64 bytes and have created my USB buffer[...

LMorr.3 by Senior II
  • 2257 Views
  • 2 replies
  • 0 kudos

STM32 RS485通讯 - 在2.5Mbps波特率下可以接收数据吗?

STM32F051C8T6产品,想用来和多摩川的编码器产品通讯,发送数据0x02,多摩川编码器发送6个字节返回。但用6个字节的中断得不到数据,用6个字节读取也无法得到数据。中断只能收到一个字节,02。有指导问题出在哪里了?

caixf by Associate II
  • 1604 Views
  • 1 replies
  • 0 kudos

Change Flash Standard Boot Startup Adress with STM32ide

 using stm32ide and a stm32f407 I would like to change the boot address to 0x8000000 to leave the first 4 sectors free from 0x4000 to position the boot at 0x8010000 I made a series of settings (not sufficient). in flash.ld file change1) FLASH (rx) : ...

Resolved! STM32F411E-DISCO and MCP2515 INTERRUPT

Hello, by connecting an mcp2515 to Stm32, I enabled it to communicate properly with other cards via the Can network. However, when a message arrives, I couldn't understand how to receive it with the INT pin and I couldn't do it. I tried connecting th...

sheqom by Associate III
  • 3705 Views
  • 4 replies
  • 0 kudos

Resolved! stm32h7 lwip sdmmc1 fatfs

Hi,Is there any sample for H755 with lwip eth and sdmmc1 fatfs?.How configure the MPU region?. Thanks,    

GPHIL.1 by Associate II
  • 3102 Views
  • 3 replies
  • 0 kudos

STSPIN32G4 as 600V Version

HelloFor future blower motors in our products, we are currently using the STSPIN32F0602. Unfortunately, memory space is very limited and we would like to use the STSPIN32G4 in order to introduce new products that are as future-proof as possible. Howe...

Thomi by Associate
  • 879 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H730 ETH receive not working

Hi all,For the last couple of weeks I've been trying to deal with receiving an ETH frame from PHY on my own PCB design with STM32H730VBT.To make sure the firmware is OK I took a Nucleo-H723ZI (CPU from the same family) and configured it to work with ...

e1.png e2.png e3.png e4.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.