2018-08-10 2:49 AM
On Reference Manual RM0008, pag 186, bit 2, Alternate Function I/O Remap, it stats that the only available pairs for Usart 1 RX/TX can be PA9/PA10 or PB6/PB7, but on the pinout image for the same NUCLEO-F103RB the Usart 1 pinout is on PA2/PA3.
Which one of the two is wrong?
2018-08-10 5:03 AM
USART2 uses PA2/PA3
2018-08-10 6:00 AM
Hello,
On the pinout: USART2_TX is on PA2 and USART2_RX is on PA3.
You can also check the pin definitions in the STM32F103 datasheet.
With Regards,
Imen
2018-08-10 6:00 AM
Hello,
On the pinout: USART2_TX is on PA2 and USART2_RX is on PA3.
You can also check the pin definitions in the STM32F103 datasheet.
With Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.