2018-07-13 1:16 PM
I'm using STM32CubeProgrammer CLI on Ubuntu 18.04 to program an STM32F413VHT6. Often times, the STM32CubeProgrammer fails with 'Error: Failed to download the File'.
If I attach the ST-Link to a Windows VM, I can successfully program the STM32F413VHT6 with the STVP software.
Here is a complete log of the CLI output:
STM32_Programmer_CLI -c port=SWD -d ******.hex -v -s
------------------------------------------------------------------- STM32CubeProgrammer v1.0.0 -------------------------------------------------------------------ST-LINK Firmware version : V2J29M18
SWD frequency = 4000 KHzConnection mode: NormalDevice ID: 0x463Device name: STM32F413/423
Device type: MCUDevice CPU : Cortex_M4Memory Programming ...Openeing and parsing file: ******.hex File : ******.hex Size : 284896 Bytes Address : 0x08004000Erasing memory corresponding to segment 0:Erasing internal memory sectors [1 6]Erasing memory corresponding to segment 1:Erasing internal memory sector 9Download in Progress:Error: Failed to download Segment[0]Error: Failed to download the FileTime elapsed during the download operation is: 00:00:42.754VERIFYING ...Read progress:[==================================================] 100%Error: Verification issue at address 0x08004000 (byte = 0xFF)
Error: Download verification failedRUNNING Program ...
Address: : 0x8000000Application is runningStart operation achieved successfully2018-08-09 10:52 PM
A new version has been posted, you might want to try that and report if it still gives you issues.
2018-08-10 5:59 AM
Hi @Jonathan Goldberg ,
I couldn't reproduce your issue on window and linux (see attached file).
It could be related to write protection in the option bytes. Please verify that there's no write protection in the option bytes?
If you still have the issue even after the the option bytes check, please provide the hex file you're using?
Khouloud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.