2014-01-31 8:14 AM
Hi,
I have a problem with i2c interface of stm32f103rbt6 mcu. I use interrupts for sending/receiving data, and everything is ok until slave (MS5611) sent 3 bytes. The bytes are received correctly, but i2c interface is death after this operation. You can see whole transmission in attached i2c_1.png file. The packed labaled as ''2'' is detailed in file i2c_2, it's just receiving of 3 bytes. After that I try to send 1 byte (same like packed labaled as 1), but the i2c interface sends only the start and end sequence. Only one event is trigered case I2C_EVENT_MASTER_MODE_SELECT: // EV5 // sending addres and set transmiter mode I2C_AcknowledgeConfig(I2C1, ENABLE); I2C_Send7bitAddress(I2C1, gv_i2c1_addr, I2C_Direction_Transmitter); What do I wrong? Thank you in advance Krzysiek #stm32 #i2c2014-01-31 8:42 AM
Hi
''I have a problem with i2c interface of stm32f103rbt6 mcu. I use interrupts for sending/receiving data, and everything is ok until slave (MS5611) sent 3 bytes. The bytes are received correctly, but i2c interface is death after this operation.'' I think it is because you have pushed the I2C peripheral into an unknown state. Your I2C transmission for a Master to Slave read is not correct. See : http://en.wikipedia.org/wiki/I2c For the master to read bytes from a slave - it must first send the slave address + write, set up the read address, no byte etc. Then it must send a re-start and the slave address + read, then the slave can reply.2014-01-31 10:12 AM
Hi Chen Chung,
Sorry, but you are wrong. There are simple i2c devices, without registers, so i2c sequence is much simpler then you think ;). Please compare MS5611 data sheet with files attached by me. Everything is ok, and I could read the prom, start conversion, read the results, but only one time. After reading results (3 bytes) the i2c interface stops working. Regards KrzysiekWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.