STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flash programming

Posted on February 01, 2014 at 14:38Hi All,I am working on STM32F103.When I program the device using system boot loader I save also some user data at the address 0x9800.Now I would like to re-program these data with the on-line application using FLA...

sirpak by Associate II
  • 1563 Views
  • 5 replies
  • 0 kudos

Keil MDK 5 RTOS and ST STM32F4xx_DSP_StdPeriph_Lib

Posted on January 27, 2014 at 17:51Does anyone know if it's possible to use functions from the STM32F4xx_DSP_StdPeriph_Lib in a project built with Keil MDK 5 and using the CMSIS RTOS and Keil middleware please? I cannot use the STM32F4xx_DSP_StdPeri...

John F. by Senior
  • 1000 Views
  • 3 replies
  • 0 kudos

Timer/PWM Question

Posted on February 01, 2014 at 01:59I have tried searching through the web, as well as the forum, as well as the Programming Manuals for various STM32F4 devices, but I cannot seem to get a good description of what TIM_ClockDivision in the TimeBaseSt...

Reset device peripherials after remapping

Posted on January 31, 2014 at 15:38Hey guys, I am already running an application with USB in VCP mode, and I developed a circuit, that would rise voltage on boot0-pin to enter the bootloader after a reset is done trough the watchdog... My problem is...

stm32 i2c problem after reciving 3 bytes

Posted on January 31, 2014 at 17:14Hi, I have a problem with i2c interface of stm32f103rbt6 mcu. I use interrupts for sending/receiving data, and everything is ok until slave (MS5611) sent 3 bytes. The bytes are received correctly, but i2c interface...

STM32F4 in package 3 x 3 mm

Posted on January 30, 2014 at 22:24Hi all! The STM32F401 http://www.st.com/web/en/catalog/mmc/FM141/SC1169/SS1577/LN1810?ecmp=ln1810_enews_ln1810_jan2014&sp_rid=NjkwODIzNDM5MTMS1&sp_mid=8196895 contains information about new MCUs in small 3x3mm pack...

ryabokon by Associate
  • 1814 Views
  • 5 replies
  • 0 kudos

stm32 I2c no kommunikation

Posted on November 10, 2011 at 14:38Hi, i try to let two stm32 Boards set all 2 seconds  a few bytes on the general call bus (0x00). Every board allone is doing his job, but when i put them together at the bus, there is nothing going on the I2C bus....

STemWIN + CooCox CoIDE

Posted on September 03, 2013 at 10:47Hello everybody, I would like to try STemWIN library with CoIDE environment. I check that the examples only for the payed license tools. I try set up the CoiDE project but I've linker errors.        [cc] c:/progr...

totti001 by Associate II
  • 4308 Views
  • 9 replies
  • 0 kudos

.NET Micro Framework for 429iDiscovery

Posted on January 28, 2014 at 15:23Hi everybody.I just downloaded and flashed .NET Micro Framework provided by ST, at link http://www.st.com/web/en/catalog/tools/PF260087 (UM1676).Board boots fine, bu after having installed USB Driver (after having ...

maiorfi by Associate II
  • 1189 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.