2025-04-24 1:16 PM - last edited on 2025-04-29 9:52 AM by Andrew Neil
Is the internal bootloader on the STM32H723 DO-178 certified? It just dawned on me that the whole line of CPUs might be disqualified for aircraft use because the bootloader code "flies" with the aircraft and all such code must be certified to the level declared by the system (DAL levels A-D). Do you have avionics customers that use these? Can the bootloader be erased?
Regards,
Mark
Solved! Go to Solution.
2025-04-28 11:02 AM
No Pavel, that is completely incorrect. I am addressing embedded avionics equipment that is most certainly connected to the avionics system. Your PC is not DO-178 avionics software. This whole dioscussion is based on using an STM32 in avionics systems.
2025-04-28 12:12 PM
The bootloader is never activated or accessed unless you physically boot it into bootloader mode.
Like @Pavel A. said, it's passive. You have the option to write your own bootloader and get it certified.
2025-04-29 1:22 AM
Then, pity. The STM32 is removed from flight ((
2025-04-29 8:10 AM
If it's there it can be executed and therefore subject to certification criteria. The FAA doesn't F-around when it comes to safety-critical systems.
2025-04-29 9:15 AM
Sounds like it would be a hardware design issue if the FAA can physically get the built bootloader to run, unless they do a hardware modification to do so.
Would you trust the FAA to certify code versus accidently getting the bootloader to run? They can't even manage the airspace without planes nearly colliding into each other, or helicopter mishaps.
2025-04-29 10:20 AM
Hi Karl,
Thank you for trying to help but you need some DO-178 experience to ask relevant questions on this subject.
Regards,
Mark
2025-04-29 10:35 AM
And yet, you're the OP asking question on the matter.
2025-04-29 2:12 PM
What's your point? I was asking if it was pre-certified?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.