2025-04-24 1:16 PM - last edited on 2025-04-29 9:52 AM by Andrew Neil
Is the internal bootloader on the STM32H723 DO-178 certified? It just dawned on me that the whole line of CPUs might be disqualified for aircraft use because the bootloader code "flies" with the aircraft and all such code must be certified to the level declared by the system (DAL levels A-D). Do you have avionics customers that use these? Can the bootloader be erased?
Regards,
Mark
Solved! Go to Solution.
2025-04-25 4:29 PM - last edited on 2025-04-29 9:39 AM by Ted THOMPSON
Hello @Niramas
This post has been escalated to the ST Online Support Team for additional assistance.
Regards.
Roger
2025-04-24 11:57 PM
For unmanned avionics (aka drones) be assured that people use STM32H7's and have no complaints about the internal bootloader.
> Can the bootloader be erased?
No, unfortunately.
2025-04-25 6:17 AM
Hi @Niramas ,
Our current STM32 MCUs are general purpose ones and not qualified for aircraft usage.
This post has been escalated to the ST Online Support Team for additional assistance. They may contact you directly in case they have some farther information to add.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-25 6:21 AM
The question has to do with FAA certification, not whether it works.
2025-04-25 6:25 AM
Thank you for the response. Can you verify that the BL area cannot be erased? Can it come unprogrammed by special order? This question matters in that we have product that would be OK at low verification levels (e.g. controlling seat positions) but would be disqualified at higher safety levels (e.g. controlling landing gear).
2025-04-25 8:08 AM
As already answered by Pavel, the BL area cannot be erased.
Special orders should be discussed with Sales, better to submit your complete request in OLS in this case.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-25 2:31 PM
Would it help to know that STM32H7 can be programmed so that the internal bootloader is never activated? (both boot addresses are set to the user app)
2025-04-25 4:29 PM - last edited on 2025-04-29 9:39 AM by Ted THOMPSON
Hello @Niramas
This post has been escalated to the ST Online Support Team for additional assistance.
Regards.
Roger
2025-04-28 7:42 AM
The FAA expects all code that flies with the plane be certified to the safety level of the system.
2025-04-28 8:05 AM - edited 2025-04-28 8:05 AM
Well then if I fly with a laptop full of Windows and other stuff, do I have to certify it? If the answer is no because it is not connected to the systems, then the passive part of STM32 firmware is not connected too.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.