2024-07-31 1:39 AM
hello, where can i download win11 STM virtual com port? i install both VCP_V1.5.0_Setup_w7_x64_64bits and W8_x86_32bit all not working ! i din see
STM Virtual Com port at device manager! only STM STLink visual com port appear ...
2024-07-31 8:05 PM
yes.. i hav a program but seems its not working,,,
2025-03-27 3:56 AM
I am facing similar issue , STM Virtual Com port not appearing at device manager when I plug usb cable . Were you able to resolve this?
2026-03-18 4:23 AM
Having similar issues with the EVL6482H-Discovery board, latest firmware flashed shows up as a HID compliant barcode reader under windows 11.
HID\VID_0483&PID_7004&REV_0110
HID\VID_0483&PID_7004
HID\VID_0483&UP:008C_U:0001
HID_DEVICE_UP:008C_U:0001
It identifies as a HID compliant device with 2 endpoints
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.