2017-06-28 10:36 PM
Dear all good ST people,
I am building GUI for machine using emwin GUI builder given by ST for first time. i m able to generate the desired GUI but when i add my own event-handler in this GUI, then that event-handler refuses to work at all. I m committing some mistakes which i m unable to trace. Please! help me to resolve the problem. I m attaching the required files with their description.
1. main.c: Here 3 important functions are called as written as below:
GUI_Init(); /* Initialize the Graphics Component */
CreateFramewin(); GUI_Exec(); /* Execute all GUI jobs ... Return 0 if nothing was done. */2. touchscreen.c: This File contains the code which scans the input for button shown on GUI from touch controller.3. FramewinDLG.c: This File draws the frame on LCD generated from GUI-BUILDER.
4. 20170628_174046.jpg: This File contains the screenshot of generated GUI from GUI-BUILDER.
BUTTONS SHOWN IN SCREENSHOT DON'T CHANGE BIG NUMBER '50' WHEN PRESSED AS SHOWN IN GENERATED IN GUI.
2017-07-02 2:36 AM
Easy solution in 6 steps:
:(
in the callback handlerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.