STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I use Interrupt transfer?

Posted on July 02, 2017 at 17:07Hello!I use STM32F429ZI. I have generated project with help of Cube MX. I have chosen CDC Virtual COM port. It includes two function: Transmit and Receive. Bulk IN and Bulk Out. I add Interrupt IN endpoint and I want ...

z1060 by Associate II
  • 1470 Views
  • 2 replies
  • 0 kudos

X-CUBE-CRYPTOLIB download problem

Posted on July 03, 2017 at 07:43Hello,I requested the download of X-CUBE-CRYPTOLIB and received the download link via email.When i click this link, it takes me to the X-CUBE-CRYPTOLIB product page, where I can request the software again but I can no...

Resolved! What is the COMP2_INM4 pin for in STM32F303C6 COMP module?

Posted on June 28, 2017 at 14:06The STM32F303C6 has COMP peripherals COMP2, COMP4 & COMP6.Each of these comparators have a positive (INP) and negative (INM) input pin and an output (OUT) pin.Furthermore the data sheet specifies for each comparator a...

HAL_UART_Transmit_IT(); Issue

Posted on July 03, 2017 at 00:53Hello everybody, I just got into STM32 development and using the HAL library primarily for my developments now. I am having a issue with UART IT library function. Why when I have a for loop delay or HAL_Delay in my ma...

USB MSC on internal FLASH and file deletion

Posted on July 02, 2017 at 22:16Hi to all.I'm using STM32L072 family MCU. I configured it to use last portion of internal flash (64kB) as USB MSC. It seems to work (more or less). Operative System can see it as removable drive. I can't format it but...

How to properly use HandleTypeDef in librairies

Posted on July 02, 2017 at 17:09Hello,I have a temperature sensor connected to the I2C1 bus of my board. To help me with basic configuration I use STM32 Cube to generate the base of my code. I usually then go on to write my own libraires to use at l...

FLASH-USART-FLASH (Circular)

Posted on July 02, 2017 at 16:30FLASH-USART-FLASH  (Circular)hallo guys ,I have one assignment ,that i have to read array of data from FLASH memory and send it through the USART  after that I have to send array of data through DOCKLITE and store it ...

STemwin Guibuilder on STM32F746-DISCOVERY BOARD

Posted on June 29, 2017 at 07:36Dear all good ST people,                                        I am building GUI for machine using emwin GUI builder given by ST for first time. i m able to generate the desired GUI  but when i add my own event-handl...

Resolved! STM32F031 uart bootloader signal levels

Posted on June 30, 2017 at 20:20I have a design where another micro is connected to the STM32F031 UART pins and I am attempting to enter the rom bootloader.  I referenced AN3155 for details on how the bootloader works, however, there is no definitio...

UART problem on L452RE

Posted on June 30, 2017 at 13:43Hello guys,I am still working on a LoRa node on the basis of a Nucleo board. It seems as nobody knows how the LoRa middelware can be ported, to use for example a SX1272 shield https://community.st.com/0D50X00009XkXhMS...

Jonas Chr by Associate II
  • 2832 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.