2019-04-14 12:39 PM
Hello,
I am working on a project with a STM32F469 Disco using STemWin.
For configuration of a lot of settings I have designed a GUI menu structure with about 10 different windows created by the emWin GUIBuilder.exe.
Jumping between these windows works fine.
After configuring is finished I am starting one the main tasks of the program by pressing a GUI-Button in my GUI-main-menu.
Cause I don't want to have undefined delays by the dialogs in my main tasks, I am exiting the windows-manager with:
GUI_EndDialog(pMsg->hWin, 0);
hItem = pMsg->hWin;
WM_DeleteWindow(hItem);
GUI_Clear();
Within the main task I write some text directly to the LCD by: GUI_DispStringAt.. or GUI_DispDecAt...
After the main task is done I reenter the GUI by:
GUI_Exit();
HAL_Delay(100);
GUI_Init();
...and then start the GUI again by: hWin = GUI_CreateDialogBox...
This works also fine for exactly 9 times.
When the GUI is reentered the 10th time, I won't work again.
The funny thing is, that the GUI does not really crash in a hardfault or so. It is still running and shows me, that I press a GUI-button by changing the color of it. But the code which is written in the "case WM_NOTIFICATION_RELEASED..." section is not executed anymore. (...but it worked for the first 9 times...)
This also happens if I start different main tasks with different buttons. Exactly after 9 starts together (for example 4x task 1 and 5x tast 2) it stucks.
When I halt the program by the debugger I find it always in
void GUI_X_Delay(int ms)
{
int tEnd = OS_TimeMS + ms;
while ((tEnd - OS_TimeMS) > 0);
}
It seems, that it doesn't come to the
static void _cbDialog(WM_MESSAGE * pMsg) { ....
anymore.
Does anybody has an idea to solve this issue?
The values of
GUI_ALLOC_GetNumUsedBytes()
GUI_ALLOC_GetNumFreeBytes()
stays constant for all the 9 cycles
I just updated to the latest STemWin. I work with Atollic on a Win10 PC.
Thanks for your replies
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.