2017-07-02 7:30 AM
FLASH-USART-FLASH (Circular)
hallo guys ,
I have one assignment ,
that i have to read array of data from FLASH memory and send it through the USART after that I have to send array of data through DOCKLITE and store it in FLASH and when i remove and plug in again the what ever array of data is in FLASH i have send through USART .
flow is 1. read array from FLASH
2.send through USART to DOCKLITE-
3.NOW DOCKLITE send data one by one
4. store in data in FLASH
5. READ array from FLASH
guys any idea how to do it ...
2017-07-02 8:21 AM
Start with the elements of the problem you understand how to implement, or do mostly, and then extend and expand from there.
Discuss with the person setting the assignment.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.