2011-08-02 5:35 AM
I am trying to get started with IAR EWARM 6.21 on the eval board. It includes a variety of sample projects, and they of course seem to compile and link properly. I have set the debugger options to use ST-LINK, but when I attempt to download and debug, I get a ''Fatal error: ST-Link Connection error'' dialog. I started with the default ST-LINK settings, and have tried a number of others, and all I get is the same error.
One would think I am missing something trivial, yet essential... Any ideas? Thanks2011-08-05 6:23 AM
Hi,
Please download the last ST-LINK utility software (V2.0) from this link:http://www.st.com/internet/com/SOFTWARE_RESOURCES/TOOL/DEVICE_PROGRAMMER/um0892.zip
, execute it, configure your toolchain debugger to use STLink, place the JP18 (jumper) on the right position (stlk). And it should works. Cheers, STOne-32.2011-09-24 11:29 PM
Hi,
I have the same problem like Robert with the STM32VLDISCOVERY and IAR6.20. After Download and Debug I get the following: Loaded macro file: C:\Programme\IAR Systems\Embedded Workbench 6.0 Evaluation\arm\config\flashloader\ST\FlashSTM32F10xxx.mac Fatal error: ST-Link Connection error Session aborted! Failed to load flash loader: C:\Programme\IAR Systems\Embedded Workbench 6.0 Evaluation\arm\config\flashloader\ST\FlashSTM32F10xxxRAM6K.out Failed to load flash loader: C:\Programme\IAR Systems\Embedded Workbench 6.0 Evaluation\arm\config\flashloader\ST\FlashSTM32F100xB.flash This only happens on my notebook computer, on my desktop everything is fine. I've already tried the ''um0892.zip'' trick, doesn't help. Any suggestions?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.