2018-12-03 4:02 AM
Hello there,
I am trying to connect to a stm32F091 mcu through st-link_cli. The problem appears when the CLI cannot recognice the device, but when I use the STM32 ST-Link Utility (the one with GUI) there are no problem in find the device. Anyone could help me?
This is what i am writing in cmd
And this is what i get with the GUI:
2018-12-03 4:05 AM
Okey seems to not appear the image i attach so i write it by myself:
"This is what i am writing in cmd"
$PATH\ST-LINK_CLI.exe -c SWD
STM32 ST-LINK_CLI v1.2
STM32 ST-LINK Command Line Interface
Connected via SWD
Device ID:0x442
Device Family: Unknown device
"And this is what i get with the GUI:"
13:05:41 : ST-LINK SN : 48FF77067266535206261867
13:05:41 : ST-LINK Firmware version : V2J32S7
13:05:41 : Connected via SWD.
13:05:41 : Connection mode : Normal.
13:05:41 : Debug in Low Power mode enabled.
13:05:42 : Device ID:0x442
13:05:42 : Device flash Size : 256KBytes
13:05:42 : Device family :STM32F09xx
thank you every one
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.