STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BFB2 and bootloader flash-bank selection

Posted on February 23, 2016 at 18:15I've recently delved into this subject because I need to design a firmware upgrade mechanism on the STM32L4xx.  The documentation is pretty much useless, as it is not only incomplete, but contradictory too.  I'm g...

mhaun by Associate II
  • 10716 Views
  • 14 replies
  • 1 kudos

STM32L475RC RTC Issue?

Are there any known issues with the RTC Wakeup on the STM32L475?I cannot get it to work, I've copied the code exactly as it appears in the STOP2_PWR example, but no matter what I do the ISR does not get called.If I check the registers I can see the t...

adrian by Associate III
  • 2109 Views
  • 3 replies
  • 0 kudos

Is SafeRTOS support in STM32CUBEMX?

If I want to use the SafeRTOS for critical issue can I use it in the cubeMX as I use today the FreeRTOS?If it is possible or not at this stage, and if yes what adaptation do I need to do to use it?Is there any guide for immigrate Safe RTOS to CUBEMX?...

Barbie by Associate II
  • 1290 Views
  • 1 replies
  • 0 kudos

STM32G0 Series Information

I noticed a new STM32G0 series (Cortex-M0+ core) support in the latest STM32CubeMX. Is there any information available to general public about this new series? Thanks.

ST-LINK_CLI.exe Family device :Unknown device

Hello there,I am trying to connect to a stm32F091 mcu through st-link_cli. The problem appears when the CLI cannot recognice the device, but when I use the STM32 ST-Link Utility (the one with GUI) there are no problem in find the device. Anyone coul...

MP??r by Associate
  • 1367 Views
  • 1 replies
  • 0 kudos

Any sample projects Using stm32 F407g-disc1 board

Guys this is very popular board. Is there any good source where projects are made using this board(I mean using the peripheral available on this board) are available? So simple applications, Using C or C++? Any IDE.

MRana by Associate II
  • 1584 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.