2023-07-11 10:17 AM - edited 2023-07-11 10:20 AM
As described.
I am using the B-U585I-IOT02A Discovery development kit. Just testing basic SPI operation and trying to use all three SPI lines.
Using basic setup with STM Cube ID I can send data using HAL_SPITransmit over SPI1 and SPI2. Trying to do the same on SPI3 returns an error. I also do not see any signals when probing SCK and MOSI on SPI3 when using an oscilloscope.
Am I missing something here? Or is there maybe a deeper issue?
Test code (SPI3 call returns an error, due to lack of EOT flag resulting in a timeout:
Setup code (seems to be the same for each SPI instance...) generated by STMCube:
/**
* @brief SPI MSP Initialization
* This function configures the hardware resources used in this example
* hspi: SPI handle pointer
* @retval None
*/
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(hspi->Instance==SPI1)
{
/* USER CODE BEGIN SPI1_MspInit 0 */
/* USER CODE END SPI1_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SPI1;
PeriphClkInit.Spi1ClockSelection = RCC_SPI1CLKSOURCE_SYSCLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* Peripheral clock enable */
__HAL_RCC_SPI1_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
/**SPI1 GPIO Configuration
PE14 ------> SPI1_MISO
PE13 ------> SPI1_SCK
PE15 ------> SPI1_MOSI
*/
GPIO_InitStruct.Pin = GPIO_PIN_14|GPIO_PIN_13|GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/* USER CODE BEGIN SPI1_MspInit 1 */
/* USER CODE END SPI1_MspInit 1 */
}
else if(hspi->Instance==SPI2)
{
/* USER CODE BEGIN SPI2_MspInit 0 */
/* USER CODE END SPI2_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SPI2;
PeriphClkInit.Spi2ClockSelection = RCC_SPI2CLKSOURCE_SYSCLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* Peripheral clock enable */
__HAL_RCC_SPI2_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/**SPI2 GPIO Configuration
PD4 ------> SPI2_MOSI
PD3 ------> SPI2_MISO
PD1 ------> SPI2_SCK
*/
GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_3|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/* USER CODE BEGIN SPI2_MspInit 1 */
/* USER CODE END SPI2_MspInit 1 */
}
else if(hspi->Instance==SPI3)
{
/* USER CODE BEGIN SPI3_MspInit 0 */
/* USER CODE END SPI3_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SPI3;
PeriphClkInit.Spi3ClockSelection = RCC_SPI3CLKSOURCE_SYSCLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* Peripheral clock enable */
__HAL_RCC_SPI3_CLK_ENABLE();
__HAL_RCC_GPIOG_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/**SPI3 GPIO Configuration
PG9 ------> SPI3_SCK
PD6 ------> SPI3_MOSI
PG10 ------> SPI3_MISO
*/
GPIO_InitStruct.Pin = GPIO_PIN_9|GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI3;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/* USER CODE BEGIN SPI3_MspInit 1 */
/* USER CODE END SPI3_MspInit 1 */
}
}/* USER CODE BEGIN 2 */
uint8_t tx_data1[] = {1, 1, 1, 1};
HAL_StatusTypeDef status1 = HAL_ERROR;
uint8_t tx_data2[] = {2, 2, 2, 2};
HAL_StatusTypeDef status2 = HAL_ERROR;
uint8_t tx_data3[] = {3, 3, 3, 3};
HAL_StatusTypeDef status3 = HAL_ERROR;
(void)status1;
(void)status2;
(void)status3;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
status1 = HAL_SPI_Transmit(&hspi1, tx_data1, sizeof(tx_data1), 10); // Returns ok
status2 = HAL_SPI_Transmit(&hspi2, tx_data2, sizeof(tx_data2), 10); // Returns ok
status3 = HAL_SPI_Transmit(&hspi3, tx_data3, sizeof(tx_data3), 10); //Returns error!
__NOP();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
Solved! Go to Solution.
2023-07-11 12:07 PM
I solved the issue.
SPI clock pin was PG9, which is in the VDDIO2 power domain. I enabled VDDIO2 power with the HAL_PWREx_EnableVddIO2() function and this solved the problem.
It was not really related to SPI. Even trying to use PG9 as a regular GPIO without enabling VDDIO2 did not work.
2023-07-11 12:07 PM
I solved the issue.
SPI clock pin was PG9, which is in the VDDIO2 power domain. I enabled VDDIO2 power with the HAL_PWREx_EnableVddIO2() function and this solved the problem.
It was not really related to SPI. Even trying to use PG9 as a regular GPIO without enabling VDDIO2 did not work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.