2017-06-09 5:08 AM
why spi1 is not starting in my controller.
here below is my code
#include 'stm32f10x.h'
#include 'stm32f10x_rcc.h'
#include 'stm32f10x_gpio.h'
#include 'stm32f10x_spi.h'
#define SPIx_RCC RCC_APB2Periph_SPI1
#define SPIx SPI1
#define SPI_GPIO_RCC RCC_APB2Periph_GPIOA
#define SPI_GPIO GPIOA
#define SPI_PIN_MOSI GPIO_Pin_7
#define SPI_PIN_MISO GPIO_Pin_6
#define SPI_PIN_SCK GPIO_Pin_5
#define SPI_PIN_SS GPIO_Pin_4
SPI_InitTypeDef SPI_InitStruct;
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitTypeDef GPIO_InitStructure;
//SPI_InitTypeDef SPI_InitStructure;
#define BufferSize 32
#define SEND_LIMIT 3
uint8_t SPIz_Buffer_Tx[BufferSize] = {0x1, 0x2, 0x4, 0x54, 0x55, 0x56, 0x57,
0x58, 0x59, 0x5A, 0x5B, 0x5C, 0x5D, 0x5E,
0x5F, 0x60, 0x61, 0x62, 0x63, 0x64, 0x65,
0x66, 0x67, 0x68, 0x69, 0x6A, 0x6B, 0x6C,
0x6D, 0x6E, 0x6F, 0x70};
__IO uint8_t TxIdx = 0, RxIdx = 0, k = 0;
void SPIx_EnableSlave()
{
// Set slave SS pin low
SPI_GPIO->BRR = SPI_PIN_SS;
}
void SPIx_DisableSlave()
{
// Set slave SS pin high
SPI_GPIO->BSRR = SPI_PIN_SS;
}
void SPIx_Init()
{
/* Initialize LED which connected to PC13 */
// Enable PORTC Clock
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);
/* Configure the GPIO_LED pin */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
//GPIO_SetBits(GPIOC, GPIO_Pin_13); // Set C13 to High level ('1')
GPIO_ResetBits(GPIOC, GPIO_Pin_13); // Set C13 to Low level ('0')
// Step 1: Initialize SPI
RCC_APB2PeriphClockCmd(SPIx_RCC, ENABLE);
SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_128;
SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge;
SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low;
SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStruct.SPI_Mode = SPI_Mode_Master;
SPI_InitStruct.SPI_NSS = SPI_NSS_Soft | SPI_NSSInternalSoft_Set;
SPI_Init(SPIx, &SPI_InitStruct);
SPI_Cmd(SPIx, ENABLE);
// Step 2: Initialize GPIO
RCC_APB2PeriphClockCmd(SPI_GPIO_RCC, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
// GPIO pins for MOSI, MISO, and SCK
GPIO_InitStructure.GPIO_Pin = SPI_PIN_MOSI | SPI_PIN_SCK;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;//GPIO_Mode_Out_PP;//
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(SPI_GPIO, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = SPI_PIN_MISO ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;//GPIO_Mode_Out_PP;//
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(SPI_GPIO, &GPIO_InitStructure);
// GPIO pin for SS
GPIO_InitStructure.GPIO_Pin = SPI_PIN_SS;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(SPI_GPIO, &GPIO_InitStructure);
// Disable SPI slave device
SPIx_DisableSlave();
}
uint8_t SPIx_Transfer(uint8_t data)
{
// Write data to be transmitted to the SPI data register
SPIx->DR = data;
// Wait until transmit complete
while (!(SPIx->SR & (SPI_I2S_FLAG_TXE)));
// Wait until receive comple
while (!(SPIx->SR & (SPI_I2S_FLAG_RXNE)));
// Wait until SPI is not busy anymore
while (SPIx->SR & (SPI_I2S_FLAG_BSY));
// Return received data from SPI data register
return SPIx->DR;
}
int main(void)
{
int i;
SPIx_Init();
while (1) {
GPIOC->ODR ^= GPIO_Pin_13; // Invert C13
SPIx_EnableSlave();
/* delay */
for(i=0;i<0x100000;i++);
// SPIx_Transfer('1');
while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET)
{
}
/* Send dummy data */
SPI_I2S_SendData(SPI1, 'b');
// SPI_I2S_SendData (SPI1,0xff);
for(i=0;i<0x100000;i++);
SPIx_DisableSlave();
/* Toggle LED which connected to PC13*/
GPIOC->ODR ^= GPIO_Pin_13;
/* delay */
for(i=0;i<0x100000;i++);
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
#stm32-f
2017-06-09 5:51 AM
Hi
no36
,-Nesrine-
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.