2014-02-10 1:39 AM
Hi
I'm using STM32F373x SPI in slave mode. I get errors in about 0.1% bits transmitted, occurs in 50% of units from first production series of custom board. SPI lines have RC filter installed to improve EMC immunity. Rise/fall times are about 1us with filters and 10ns without them. I get no errors without filters. My question is what parameter do I exceeded?Table 58 defines max. rise/fall 8ns (I guess only for master, cause load is also described). I think I'm not getting out of 30-70% duty cycle. Speed is 190kHz, reducing to 80kHz didn't changed anything. #eye-pattern #stm32-spi2014-02-13 5:24 AM
waclawek.jan:
Many thanks for detailed information.I knew that SPI is not intended for longer distances and we could live with this cheap and fast medium for our purposes. I never thought about it, I guess SPI hardware has some more hysteresis. I'll keep it in mind for future projects.Today I can't recreate this errors (using exactly the same hardware and power supplies as for last week). I'll write when we decide which solution is sufficient for our needs.2014-02-13 5:39 AM
BTW I used similar SPI with board to board connection in older projects without problems (different uC). Now I checked details and it looks like Atmel AVR has much different (better for my purposes) Slave hardware, including clock sampling and max. Slave slope allowed 1.6us.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.