STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI RX Buffer via DMA Too Big

Posted on February 13, 2014 at 14:07I've set up my DMA to transfer 106 half-words via the SPI to a memory buffer. I am quite confident that my buffer size is correct. However, when the transfer actually occurs, it is twice the size I expect (and is ...

jvavra by Associate III
  • 4790 Views
  • 15 replies
  • 0 kudos

ADC reference voltage of stm32f4-discovery

Posted on February 13, 2014 at 14:00I use stm32f4-discovery board. I am working with the ADCs, and for my prpose I need to set the ADC reference VREF+ at 3.2V. in the reference manual RM0090 it is said that stm32f4 LQFP100 has VREF+ VDDA pin. But th...

sen2 by Associate II
  • 2318 Views
  • 3 replies
  • 0 kudos

STM3240-G USB-MSC Wrong SD Card Size

Posted on February 12, 2014 at 18:03I'm using custom code which is somewhat ported from the STM3240-G USBD-MSC example application. I also made modifications to the read/write functions to take blocks as arguments vs. bytes. I've stepped through the...

nattayb by Associate II
  • 2264 Views
  • 4 replies
  • 0 kudos

ADC frequency

Posted on February 13, 2014 at 14:11Hi all,I'm using stm32f100c8 with an external oscillator 8MHz to produce a system clock of 24MHz. All the peripherals are on the default division lines.Now the ADC1 which is with the TIM1 on PCLK2 is supposed to r...

0690X00000602rGQAQ.jpg
sherif by Associate II
  • 1231 Views
  • 1 replies
  • 0 kudos

SPI raise/fall time

Posted on February 10, 2014 at 10:39HiI'm using STM32F373x SPI in slave mode. I get errors in about 0.1% bits transmitted, occurs in 50% of units from first production series of custom board. SPI lines have RC filter installed to improve EMC immunit...

bpacan by Associate II
  • 8599 Views
  • 11 replies
  • 0 kudos

Default Interrupt priority levels and no of levels?

Posted on November 07, 2013 at 12:13Hi, I if will be great if some one clarify me the following, * What is the default interrupt priorities? When I read using either      priority4 = NVIC_GetPriority(UART4_IRQn); orpriority4 = NVIC->IP[EXTI4_IRQn];...

jonfs2000 by Associate II
  • 4729 Views
  • 3 replies
  • 0 kudos

RTC alarm handler does not want to work

Posted on February 13, 2014 at 09:34Good day,Like topic said, the alarm handler does not to work, but if I do like this:while (!RTC_GetITStatus(RTC_IT_ALRA));printf(''\nALARM''); //it worksHere is my code: int main(void){  NVIC_InitTypeDef  NVIC_Ini...

hitsumen by Associate II
  • 3260 Views
  • 6 replies
  • 0 kudos

f407 board with examples

Posted on March 15, 2013 at 08:39Hi! The Discovery board based on f407 served me as a starting point in preparing a course on the use of microprocessors for local students, which do not have much experience with hardware, but are familiar with the p...

dusan2 by Associate III
  • 2215 Views
  • 3 replies
  • 0 kudos

Bug in CAN_TransmitStatus function?

Posted on June 10, 2013 at 23:31I noticed something strange with the CAN_TransmitStatus function in the stm32f10x_can.c (V3.1.2) peripheral driver code. Most of the time it works fine but occasionally it returns the wrong status. The root cause is i...

raymartin by Associate II
  • 1281 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.