2021-05-07 6:22 AM
Hi,
I'm currently using an STM32G431 on a Nucleo-32 board, connected to an external audio ADC and transmitting ADC audio data via SPDIF, all audio stuff running with 192kHz.
Toolchain: CubeIDE, design started with CubeMX.
In the DMA TX half complete / complete ISR the ADC data is shifted and channel status bit is added.
So far, so good, works like a charm.
Yesterday I changed UART speed (the virtual COM port via the Link-MCU) from 921600 baud to 115200 baud, today I see that the channel status data is missing, although audio data is still tranmitted correctly.
As I haven't changed anything else I switched back the UART to 921k6, and surprise, channel status data is back.
Any ideas what's going on there?
2021-05-07 8:38 AM
It's the frame count offset again.
But why does that depend on the baud rate?
I stopped all UART outputs when starting SPDIF, still the same problem.
UART TX for printf is running in DMA mode, lower priority than SAI.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.