STM32H755IIT6 is in stock, is there something wrong with it?
All STM32 CPUs seem to be out stock, but this chip. Is there a reason for that. What I am worried is that is there flaws on the chip, or is it just expensive.
Ask questions, find answers, and share insights on STM32 products and their technical features.
All STM32 CPUs seem to be out stock, but this chip. Is there a reason for that. What I am worried is that is there flaws on the chip, or is it just expensive.
I checked for signals. all signals ok except PF11 / PG15 pins (RAS/CAS). Pins configured same as others dram-related: AF12, alternate function (gpio registers checked).I check this signals in GPIO mode, pins and pcb traces working well. But in altern...
Is there any documentation on the differences? Are these two part numbers functionally identical?
My code, which is in progress, stopped working with a hard fault. This is on a STM32G431 with several timers running and two dma channels. I can single step through the code with breakpoints on the timer IRQ's and the DMA IRQ's and it works for sever...
UsingSTM32CubeIDE - C/C++ 1.6.0.202101291314STM32Cube FW_H7 V1.9.0HardwareNUCLEO-H745ZI-QIS25LP128(Flash Chip)The flash is connected to QSPI bank 1 using the HAL libraries to read from an address on the flashif(HAL_QSPI_Command(&hqspi, Cmd, HAL_QSPI...
Hi,I'm currently using an STM32G431 on a Nucleo-32 board, connected to an external audio ADC and transmitting ADC audio data via SPDIF, all audio stuff running with 192kHz.Toolchain: CubeIDE, design started with CubeMX.In the DMA TX half complete / c...
Hi there everyone,I want to use SPI to communicate with an IMU, but I am having trouble communicating with any SPI devices. This is how my SPI is set. This is a snippet of my simple SPI test code./* USER CODE BEGIN 2 */ for (uint8_t i = 0;i<100;...
I am looking for a way to save a timestamp from Real-Time-Clock (RTC) with a button press, save that, and store it somewhere. How can I do this?
Posted on February 13, 2018 at 11:35Hi, just nitpicking here but still...The RM0394 (reference manual for STM32L4xxx) has a bad table of content, the entries go like this: 1, 2, 3, 4, 5, then restart 1, 2, 3, 4, 5, 6, 7, 8, then finally 1 2 3 ... as...
Hi,I'm using the STM32G473VCT6 and I'm confusing with alternate functions available in pin PB6. According to table 13 in datasheet it is possible to configure this pin as I2C1_SCL, but in table 12 this option doesn't exist. What is the correct option...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.