2020-12-03 1:16 AM
When I transmit more than 64 bytes data then its working fine and received upto 64 bytes data its working fine. I read some Documents On internet but not got clear
when I pass 100 bytes of data from host so its not working.
#define USB_HS_MAX_PACKET_SIZE 512U
#define USB_FS_MAX_PACKET_SIZE 512U //64U
#define USB_MAX_EP0_SIZE 64U
int8_t CDC_Receive_FS(uint8_t* Buf, uint32_t *Len)
{
/* USER CODE BEGIN 6 */
USBD_CDC_SetRxBuffer(&hUsbDeviceFS, &Buf[0]);
USBD_CDC_ReceivePacket(&hUsbDeviceFS);
return (USBD_OK);
/* USER CODE END 6 */
}
when I Changed the USB_MAX_EP0_SIZE =128 or 256 then USB got disable .....Kindly help me..
2020-12-03 6:32 AM
64-bytes per packet is a USB full-speed limitation/requirement. You can't change it.
2020-12-04 7:50 AM
Thank you TDK for your response .
But some times more than 64 bytes data received.
when I sent 80 bytes of data 5 to 8 times from host then it will received only ones. I used the Tera term for transmitting the data
If not possible to received more than 64 bytes data at a time then How can i received 100 bytes of data which is coming from Host. I am new in this development
Kindly help me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.