2026-03-04 6:51 PM - last edited on 2026-03-06 1:20 AM by Gyessine
I am using STM32H743 controller, LAN8720 Ethernet chip, and Keil5 programming software
I am using the IAP function of the network port and need to write the received data to FLASH. I found that the data read at that address after writing was modified. I found during debugging that after the "netif_add" function in LWIP initialization was executed, the data of my flash address was modified. May I ask what happened.
Here is my MPU configuration, I'm not sure if it's related to MPU configuration
uint8_t MPU_Set_Protection(uint32_t baseaddr, uint32_t size, uint32_t rnum, uint8_t ap, uint8_t sen, uint8_t cen, uint8_t ben)
{
MPU_Region_InitTypeDef MPU_Initure;
HAL_MPU_Disable(); // 配置MPU之前先关闭MPU,配置完成以后在使能MPU
MPU_Initure.Enable = MPU_REGION_ENABLE; // 使能该保护区域
MPU_Initure.Number = rnum; // 设置保护区域
MPU_Initure.BaseAddress = baseaddr; // 设置基址
MPU_Initure.Size = size; // 设置保护区域大小
MPU_Initure.SubRegionDisable = 0X00; // 禁止子区域
MPU_Initure.TypeExtField = MPU_TEX_LEVEL0; // 设置类型扩展域为level0
MPU_Initure.AccessPermission = (uint8_t)ap; // 设置访问权限,
MPU_Initure.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; // 允许指令访问(允许读取指令)
MPU_Initure.IsShareable = sen; // 是否共用
MPU_Initure.IsCacheable = cen; // 是否cache
MPU_Initure.IsBufferable = ben; // 是否缓冲
HAL_MPU_ConfigRegion(&MPU_Initure); // 配置MPU
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT); // 开启MPU
return 0;
}
// 设置需要保护的存储块
// 必须对部分存储区域进行MPU保护,否则可能导致程序运行异常
// 比如MCU屏不显示,摄像头采集数据出错等等问题...
void MPU_Memory_Protection(void)
{
// 保护整个内部SRAM,包括SRAM1,SRAM2和DTCM,共512K字节
MPU_Set_Protection(0x20000000, /* 基地址 */
MPU_REGION_SIZE_512KB, /* 长度 */
MPU_REGION_NUMBER0, /* NUMER1 */
MPU_REGION_FULL_ACCESS, /* 全访问 */
MPU_ACCESS_NOT_SHAREABLE, /* 允许共享 */
MPU_ACCESS_NOT_CACHEABLE, /* 允许cache */
MPU_ACCESS_BUFFERABLE); /* 允许缓冲 */
// 保护LAN8720的寄存器区域,共256字节
MPU_Set_Protection(0X30040000, /* 基地址 */
MPU_REGION_SIZE_256B, /* 长度 */
MPU_REGION_NUMBER6, /* NUMER3 */
MPU_REGION_FULL_ACCESS, /* 全访问 */
MPU_ACCESS_NOT_SHAREABLE, /* 允许共享 */
MPU_ACCESS_NOT_CACHEABLE, /* 允许cache */
MPU_ACCESS_BUFFERABLE); /* 允许缓冲 */
// 保护整个NAND FLASH区域,共256M字节
MPU_Set_Protection(0X80000000, /* 基地址 */
MPU_REGION_SIZE_256MB, /* 长度 */
MPU_REGION_NUMBER1, /* NUMER2 */
MPU_REGION_FULL_ACCESS, /* 全访问 */
MPU_ACCESS_NOT_SHAREABLE, /* 允许共享 */
MPU_ACCESS_NOT_CACHEABLE, /* 允许cache */
MPU_ACCESS_BUFFERABLE); /* 允许缓冲 */
// 保护SDRAM区域,共32M字节
MPU_Set_Protection(0XC0000000, /* 基地址 */
MPU_REGION_SIZE_32MB, /* 长度 */
MPU_REGION_NUMBER2, /* NUMER1 */
MPU_REGION_FULL_ACCESS, /* 全访问 */
MPU_ACCESS_NOT_SHAREABLE, /* 允许共享 */
MPU_ACCESS_NOT_CACHEABLE, /* 允许cache */
MPU_ACCESS_BUFFERABLE); /* 允许缓冲 */
}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.