STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MCU support both 1.8 V GPIO and 3.3 V GPIO

Hi, I am looking for MCU which support 1.8 V GPIO and 3.3 V GPIO,My target is about 20 pin 1.8 V GPIO and about 10 pin 3.3 GPIO.After my search, I think STM32F0x8 can meet my requirement.I want to know are there STM32 low power series MCU or STM32 Hi...

KSu.1 by Associate
  • 1578 Views
  • 2 replies
  • 0 kudos

STM32G030F6 / STM32G031F6 interoperability

At the moment we are struggling to get hold of any STM32G030F6's but we can get hold of STM32G031F6 chips. I've done an CUBE generation in the same pinout as the STM32G030F6 project and compared between the two projects and it looks to me that as lo...

Resolved! Why am I getting wrong internal temperature values?

Using a Nucleo STM32F091RC board, I have configured the ADC to measure all channels in a sequence, i.e. all 10 ADC pins that particular chip has, and the 3 internal ones: temperature, vrefint, vbat.I calibrated the ADC, waited the time before enablin...

SKled.1 by Senior II
  • 4442 Views
  • 5 replies
  • 0 kudos

STM32G474: Put ADC in known reset state?

My board can startup from a variety of different ways: from power-up reset, jump between application and bootloader, external watchdog reset, or software restart for other reasons.I want to ensure ADC1 and ADC2 are initialized from a clean known stat...

SPI is not working after ADC Operation

Hello,We are using STM32F2XX with ADC and external SPI Flash.In our code, there are running two threads one for ADC operation and another for Flash read write operation.We can easily use our External flash through SPI2 and ADC operation individually....

DPate.9 by Associate
  • 1993 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.