2019-12-03 12:17 PM
Here my simple code to use the encoder on STM32F746.
I have used the PI2 and PI3 of the STM32F746G-DISCO for input and volume control on an external DAC.
Probably someone could reduce the lines of code and obtain the same result.
unsigned int Enc_dir; << output direction up/down to use in the main() or in
handleTickEvent() in case of TouchGFX graphical interface
environment.
unsigned int save_a = 0, save_b = 0; << global variables
void EXTI2_IRQHandler(void)
{
uint8_t now_a;
uint8_t now_b;
HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_2);
now_a = HAL_GPIO_ReadPin(GPIOI, GPIO_PIN_2);
now_b = HAL_GPIO_ReadPin(GPIOI, GPIO_PIN_3);
if (!save_a & !save_b)
{
if (now_a)
{
save_a = now_a;
Enc_dir = 2;
}
if (now_b)
{
save_b = now_b;
Enc_dir = 1;
}
}
if (save_a & !save_b)
{
if (!now_a)
{
save_a = now_a;
Enc_dir = 1;
}
if (now_b && now_a)
{
save_b = now_b;
Enc_dir = 2;
}
}
if (save_a & save_b)
{
if (!now_a)
{
save_a = now_a;
Enc_dir = 2;
}
if (!now_b)
{
save_b = now_b;
Enc_dir = 1;
}
}
if (!save_a & save_b)
{
if (now_a)
{
save_a = now_a;
Enc_dir = 1;
}
if (!now_b)
{
save_b = now_b;
Enc_dir = 2;
}
}
}
void BSP_Encoder_Init()
{
GPIO_InitTypeDef gpio_init_structure;
__HAL_RCC_GPIOI_CLK_ENABLE();
gpio_init_structure.Pin = GPIO_PIN_2;
gpio_init_structure.Mode = GPIO_MODE_IT_RISING_FALLING;
gpio_init_structure.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOI, &gpio_init_structure);
HAL_NVIC_SetPriority(EXTI2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI2_IRQn);
gpio_init_structure.Pin = GPIO_PIN_3;
gpio_init_structure.Mode = GPIO_MODE_INPUT;
gpio_init_structure.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOI, &gpio_init_structure);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.