2015-02-23 2:15 PM
Hi everyone!
I am using st-link on stm32f0 discovery board and ST-LINK utility to program some other boards and that is working like it should. I am working with stm32f030 processor. I am wondering if it is possible to use that st-link on stm32f0 disco as debugger from IAR IDE? This is the error I get:Mon Feb 23, 2015 23:12:47: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0\arm\config\debugger\ST\STM32F05xxx_06xxx.dmac
Mon Feb 23, 2015 23:12:47: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0\arm\config\flashloader\ST\FlashSTM32F05xx8.mac
Mon Feb 23, 2015 23:12:47: ST-Link firmware too old
Mon Feb 23, 2015 23:12:47: Selecting SWD as current target interface.
Mon Feb 23, 2015 23:12:47: Hardware reset with strategy 0 was performed
Mon Feb 23, 2015 23:12:47: Initial reset was performed
Mon Feb 23, 2015 23:12:47: -I- execUserFlashInit!
Mon Feb 23, 2015 23:12:48: 276 bytes downloaded (1.73 Kbytes/sec)
Mon Feb 23, 2015 23:12:48: Loaded debugee: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0\arm\config\flashloader\ST\FlashSTM32F05xxxRAM8K.out
Mon Feb 23, 2015 23:12:48: Target reset
Mon Feb 23, 2015 23:12:48: Failed to set breakpoint at 0x20001F84 (out of breakpoints?)
Mon Feb 23, 2015 23:12:53: Debug session aborted.
Cheers,
Zlatko
2015-02-23 4:09 PM
Should be possible, you're going to want to update the firmware, as the log suggests it's old.
Get the most current ST-LINK utilities, and update with that. Then make sure to fully disconnect the target processor on the DISCO board, so it doesn't interfere. Consider the SWO and NRST pins. Review the manual, schematic, and solder bridges, etc.2015-02-24 7:48 AM
I've managed to solve the problem. I've had ''Use flash loader(s)'' box checked and it should be unchecked. It is under Project->Options->Debugger->Download.
Thank you clive for suggestions anyways ;)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.