STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 LTDC

Posted on February 25, 2015 at 20:12Hello! Sorry for my English.I try to understand the controller LTDC STM2F429.1) Maximum resolution TFT 1024x768. However, the registers of the total width and height of the display are 12 bit and 11 bits, respecti...

arlleex by Associate
  • 1078 Views
  • 2 replies
  • 0 kudos

Enable Interrupt for Blue Button on NucleoF411

Posted on February 21, 2015 at 18:14 Hello, i have a Problem or misunderstanding enabling the Interrupts for the blue button on the nucleof411 board. In short: The Interrupt is only raised when i enable EXTI15_10_IRQn, EXTI9_5_...

noah by Associate
  • 1783 Views
  • 2 replies
  • 0 kudos

STM32F4 discovery kit: cannot build example projects

Posted on February 25, 2015 at 16:00HelloI've purchased the STM32F4 discovery kit for STM32F429 and downloaded the most recent version V1.4.0 of STM32Cube.I have IAR ARM Embedded Workbench v6.70.3.I've opened the workspace D:\vt3\canview4-TM32Cube_F...

lock file

Posted on February 25, 2015 at 13:47Hello I downloaded the example of stm32f334 discovery board ; I want to change the code of the files main  file ; it is locked  read only ; I am using keil ; how can I open it ? Thank you

[SOLVED] stm32f0 discovery board as debugger

Posted on February 23, 2015 at 23:15 Hi everyone! I am using st-link on stm32f0 discovery board and ST-LINK utility to program some other boards and that is working like it should. I am working with stm32f030 processor. I am wond...

zlajoan by Associate II
  • 1494 Views
  • 2 replies
  • 0 kudos

USB devices with 2 interfaces.

Posted on June 19, 2014 at 18:02Hi guys, looking for some help with a USB device I have which has 2 interfaces. The first interface is HID, and the second is MSC. I've modified the USB Host library so that it doesn't it doesn't fail in the MSC Inter...

STM324x9I-Eval : Trace Configuration

Posted on February 23, 2015 at 23:53Hello everyone,I juste received an ulinkpro so I can use the ETM feature later on in my development.  Right now, I am trying to simply display a variable in the logic analyzer but I get no synchronization.  I read...

keaven by Associate II
  • 1286 Views
  • 3 replies
  • 0 kudos

external sdram connection to stm32f429ii

Posted on December 05, 2014 at 19:19Hi,i'd like to connect an external sdram to stm32f429ii controller. There is a question, is it necessary to use dqm pins?  i want to use MT48LC4M32B2 sdram.

Quadrature Encoder STM32 Z Capture

Posted on February 23, 2015 at 15:03 Hello,I'd like to use an quadrature encoder connected to my STM32F4 Discovery Board.I have connected the A and B outputs to PC6 and PC7. CH1 and CH2 of TIM8.It works pretty good, the timer counts.Now I'd like to...

arapp1990 by Associate II
  • 1866 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.