2022-01-05 3:14 AM
Hello Experts,
Here am using one slave which has SMBUS interface for data transmitting.
I am using STM32F103RBT6 for SM BUS and generating the code with STM CUBE MX ,but am unable generate the working code with it and its generating error code.
I updated the STM32F1 Patch and Cube Mx also still am unable to generate the code.
Does STM32F1 has SMBUS with HAL libraries?
2024-06-13 10:37 PM
Certainly! If you’re facing issues with code generation for SMBus using STM32CubeMX and the STM32F1 series, here's a step-by-step guide to help you through the process, including addressing common errors. I'll also include references to documentation and potential resources for further help.
Create a New Project:
Enable I2C Peripheral:
Configure I2C for SMBus:
Set Project and Generate Code:
“Undefined Reference to HAL_SMBUS_Init”
Cause: Missing HAL SMBus source file in your project or incorrect HAL module enabling.
Solution:
“HAL Error” During Initialization
Cause: Incorrect peripheral configuration.
Solution:
Compilation Errors Related to CubeMX Code
Cause: Potential bugs in the generated code or conflicts in configuration.
Solution:
Initialization Code (main.c):
/* I2C1 init function */
void MX_I2C1_Init(void)
{
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 100000; // Adjust as needed
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0x08; // Example own address
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
// Additional SMBus-specific initialization
hi2c1.Instance->CR1 |= I2C_CR1_SMBUS;
// Enable PEC if needed
// hi2c1.Instance->CR1 |= I2C_CR1_ENPEC;
}
Use SMBus Functions:
STM32F103 Reference Manual:
HAL Documentation:
Example Projects:
Forums and Community Help:
Here’s a simple example to perform SMBus communication:
#include "main.h"
// Define SMBus address
#define SMBUS_ADDRESS 0x1A
I2C_HandleTypeDef hi2c1; // I2C handler
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
uint8_t data[] = {0x00, 0xFF}; // Example data
if (HAL_SMBUS_Master_Transmit(&hi2c1, (uint16_t)(SMBUS_ADDRESS << 1), data, sizeof(data), HAL_MAX_DELAY) != HAL_OK)
{
// Transmission Error
Error_Handler();
}
// Additional application code
while (1)
{
// Main loop
}
}
static void MX_I2C1_Init(void)
{
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 100000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0x08;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
}
Implementing SMBus on the STM32F103RBT6 involves careful configuration in STM32CubeMX and proper initialization and handling in the generated code. Addressing errors during code generation typically involves checking your configuration, ensuring the correct inclusion of HAL modules, and updating tools. Use the provided resources and example code to verify your setup and resolve any issues. If problems persist, consulting the community or STMicroelectronics support can provide additional assistance.
2024-06-15 2:18 AM
Rama; this looks great, is there a web address for these guidelines, or should i just copy/paste into a 'local' notebook?
Danke, merçi, shukran...and thanks!
2024-12-03 12:03 AM
en.stm32cubef1-v1-8-6 There is no stm32f1xx_hal_smbus.c file
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.