2017-08-25 1:09 AM
I am following the tutorial that comes with the STM32-MAT package that deals with setting a basic block diagram to run on an STM32 target. In the simulink system I have used the predefined STM32 timer block and set it up at a frequency of 1Hz and to output an interrupt (UP) every second. The output of this block (IRQ UP) is fed as the trigger for a function call block in which I simply toggle a GPIO pin (again with the predefined STM32 GPIO_WRITE block provided in the package).
I have my code generation set to stmtlc and simulation type to 'normal'. I have set up the STMioc file with the necessary timers, interrupts and gpio ports. When I run the simulation I get an error:
An error occurred while running the simulation and the simulation was terminated Caused by: Function-call initiator 'untitled/Timers' attempted to reenable function-call subsystem 'untitled/Function-Call Subsystem' on time step '0.0'. The function-call subsystem cannot be reactivated by the same function-call initiator; there is a flaw in the implementation of the function-call initiator.
I dont understand what the issue is here.
2017-08-28 4:09 AM
Hi
Please precise which tools version are you using ?
Regards
Imen
2018-03-23 11:33 PM
I have the same problem. Does anyone have a solution?
2018-05-08 2:28 PM
I have the same problem. Does anyone have a solution?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.