2018-05-08 11:36 AM
Hi,
I have a STM3221G-EVAL board with the STM32F217IGH6 and am trying to program over CAN. I checked the revision code on the chip to see what version bootloader it has and found it was a revision '2' chip. I can't find any information though on what bootloader is on these chip revisions and whether it supports programming over CAN.. I could only find an errata sheet for this revision. Any help is appreciated, thanks.
Solved! Go to Solution.
2018-05-08 2:06 PM
Download a copy of AN2606. Refer to section 4.2 to get the memory address of where the bootloader id is. For instance on the STM32L462, the bootloader id address is listed as 0x1FFF6FFE in AN2606 which should have a low byte value of 0x92 if current. Use the following pattern in your code to retrieve that byte.
uint8_t bootLoaderVersionByte = (uint8_t)(*((uint32_t*)0x1FFF6FFE));
2018-05-08 2:06 PM
Download a copy of AN2606. Refer to section 4.2 to get the memory address of where the bootloader id is. For instance on the STM32L462, the bootloader id address is listed as 0x1FFF6FFE in AN2606 which should have a low byte value of 0x92 if current. Use the following pattern in your code to retrieve that byte.
uint8_t bootLoaderVersionByte = (uint8_t)(*((uint32_t*)0x1FFF6FFE));
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.