2018-05-08 12:03 PM
I use STM32F429IG, MT29F4G08ABADAWP that have been tested nandflash alright.
I want nandflash as usb device on WINDOWS10.
So, I setting USB_DEVICE and mass Storage Class and use example 'STM32_USB-FS-Device_Lib_V4.1.0'.
Finally, I can see USB device on WINDOWS10, but it can't express anymore information. ex) volume.
I heard, for ues this, It needs 'format' to nand flash. right?
So, how can I use it?
or What I need?
[usbd_storage_if.c]------------------------------------
int8_t STORAGE_Init_FS (uint8_t lun)
{ /* USER CODE BEGIN 2 */ return (USBD_OK); /* USER CODE END 2 */ }int8_t STORAGE_GetCapacity_FS (uint8_t lun, uint32_t *block_num, uint16_t *block_size){ /* USER CODE BEGIN 3 */ *block_num = STORAGE_BLK_NBR; *block_size = STORAGE_BLK_SIZ; return (USBD_OK); /* USER CODE END 3 */ }int8_t STORAGE_IsReady_FS (uint8_t lun){ /* USER CODE BEGIN 4 */ if(HAL_NAND_Read_Status(&hnand1) == NAND_READY) return (USBD_OK); else return (USBD_FAIL); /* USER CODE END 4 */ }int8_t STORAGE_IsWriteProtected_FS (uint8_t lun){ /* USER CODE BEGIN 5 */ return (USBD_OK); /* USER CODE END 5 */ }int8_t STORAGE_Read_FS (uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len){ /* USER CODE BEGIN 6 */ NAND_AddressTypeDef Address; Address.Plane = 0x00; Address.Block = blk_addr >> 6; Address.Page = blk_addr & 0x3F; HAL_NAND_Read_Page(&hnand1, &Address, buf, blk_len); return (USBD_OK); /* USER CODE END 6 */ }int8_t STORAGE_Write_FS (uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len){ /* USER CODE BEGIN 7 */ NAND_AddressTypeDef Address; Address.Plane = 0x00; Address.Block = blk_addr >> 6; Address.Page = blk_addr & 0x3F; HAL_NAND_Write_Page(&hnand1, &Address, buf, blk_len); return (USBD_OK); /* USER CODE END 7 */ }int8_t STORAGE_GetMaxLun_FS (void){ /* USER CODE BEGIN 8 */ return (STORAGE_LUN_NBR - 1); /* USER CODE END 8 */ }-----------------------------------------------
2018-05-08 2:43 PM
You'd need to manage the NAND at a block level, both erase, and writing partial blocks. You might need to address the read/write of multiple sectors that span the NAND block boundaries. Other thing to address would likely be ECC data, correction and wear leveling.
Windows would need to format a file system on to a blank NAND device. ie structures for FAT32, etc.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.