2022-02-07 5:49 AM
Hello,
I'm using an STM32H743-EVAL2 board, I want to access the LCD screen to draw a PNG image, so I'm using a png library to load the image, and this library use "malloc".
Unfortunately the RAM of the H743 is too small for handling large pictures, so I redirected the malloc heap to SDRAM by modifying the function _sbrk.
This is working fine, however when I try to use printf to output to UART1, the prinf calls _puts_r, which call __sinit, __sfp, __sfmoreglue, _malloc_r, _sbrk_r, and that returns an address in SDRAM, but it seems like this space allocated in SDRAM is not suitable for the function sinit because it crash (OnError_Handler is called)
If the malloc is not redirected to SDRAM, then printf is working fine.
Can someone tell me why ? and how can I make the 2 work from SDRAM ?
Thank you
2022-02-07 8:34 AM
Suggest: Two different malloc
Rename malloc in the new code to something like malloc_sdram() so it doesn't conflict with other code.
Paul
2022-02-07 4:12 PM
Perhaps instrument malloc/free to understand what's happening there, and debug what's actually failing in the C libraries.
Validate the SDRAM thoroughly, especially unaligned accesses.
Make sure the SDRAM is up early, in SystemInit() no halfway thru main()
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.