2015-03-13 12:52 AM
i am simply testing FATFS with my uSD card, whenever i write more than 800 bytes of hex data in card using f_write, it writes junk data, the hex file is attached, my code is shown below
#define size 1200uint32_t buffer[size];int main(void){ int kk; init_GPIO(); for (kk = 0; kk < size; kk++ ) { buffer[kk] = 0x12345678; } f_mount(0, &filesystem); f_open(&file, ''DATA.YUV'', FA_READ | FA_WRITE | FA_CREATE_ALWAYS); GPIOD->BSRRL = 0x1000; // this sets LED1 (green) 0x2000 0x4000 0x8000 f_write(&file, &buffer[0] , size*4, &bw); if (bw<(size*4)) while(1); f_close(&file); f_mount(0, NULL); GPIOD->BSRRH = 0x1000; GPIOD->BSRRL = 0x2000; while(1);} i am using HxD hex reader to read data,2015-03-13 1:16 AM
What functions are called by diskio.c->disk_write for writing the SD
2015-03-13 2:30 AM
2015-03-13 2:32 AM
this is the function details
SD_Error SD_WriteMultiBlocks(uint8_t *writebuff, uint32_t WriteAddr, uint16_t BlockSize, uint32_t NumberOfBlocks){ SD_Error errorstatus = SD_OK; TransferError = SD_OK; TransferEnd = 0; StopCondition = 1; SDIO->DCTRL = 0x0; if (CardType == SDIO_HIGH_CAPACITY_SD_CARD) { BlockSize = 512; WriteAddr /= 512; } /* Set Block Size for Card */ SDIO_CmdInitStructure.SDIO_Argument = (uint32_t) BlockSize; SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_SET_BLOCKLEN; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure); errorstatus = CmdResp1Error(SD_CMD_SET_BLOCKLEN); if (SD_OK != errorstatus) { return(errorstatus); } /*!< To improve performance */ SDIO_CmdInitStructure.SDIO_Argument = (uint32_t) (RCA << 16); SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_APP_CMD; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure); errorstatus = CmdResp1Error(SD_CMD_APP_CMD); if (errorstatus != SD_OK) { return(errorstatus); } /*!< To improve performance */ SDIO_CmdInitStructure.SDIO_Argument = (uint32_t)NumberOfBlocks; SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_SET_BLOCK_COUNT; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure); errorstatus = CmdResp1Error(SD_CMD_SET_BLOCK_COUNT); if (errorstatus != SD_OK) { return(errorstatus); } /*!< Send CMD25 WRITE_MULT_BLOCK with argument data address */ SDIO_CmdInitStructure.SDIO_Argument = (uint32_t)WriteAddr; SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_WRITE_MULT_BLOCK; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure); errorstatus = CmdResp1Error(SD_CMD_WRITE_MULT_BLOCK); if (SD_OK != errorstatus) { return(errorstatus); } SDIO_DataInitStructure.SDIO_DataTimeOut = SD_DATATIMEOUT; SDIO_DataInitStructure.SDIO_DataLength = NumberOfBlocks * BlockSize; SDIO_DataInitStructure.SDIO_DataBlockSize = (uint32_t) 9 << 4; SDIO_DataInitStructure.SDIO_TransferDir = SDIO_TransferDir_ToCard; SDIO_DataInitStructure.SDIO_TransferMode = SDIO_TransferMode_Block; SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable; SDIO_DataConfig(&SDIO_DataInitStructure); SDIO_ITConfig(SDIO_IT_DCRCFAIL | SDIO_IT_DTIMEOUT | SDIO_IT_DATAEND | SDIO_IT_RXOVERR | SDIO_IT_STBITERR, ENABLE); SDIO_DMACmd(ENABLE); SD_LowLevel_DMA_TxConfig((uint32_t *)writebuff, (NumberOfBlocks * BlockSize)); return(errorstatus);}2015-03-13 4:06 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.