2014-01-29 8:00 AM
Hi all;
I'm working with the discoveryF3 board, i'm using the ST-Link debugger. I want to save two float arrays into a file when debugging. My IDE is µVision4. I found that the command ''save'' can do that but when i used it, i have wrong values. Someone has an another technique to this stuff. Thanks in advance2014-01-29 8:39 AM
SAVE is pretty much the way to do this, it outputs Intel HEX format which complicates post processing a little. Then again you're using float's which should be decodable by a Windows based compiler or otherwise using the IEEE-754 format.
Other methods would perhaps to be save it onto an SD card attached to the system, or stream out via the serial port in a manner/format that suits you.2014-01-30 4:52 AM
Thank you clive1 for your quick response.
what about ''fopen'' and ''fwrite'' ? we can't use them to open and write into a file ?
2014-01-30 7:37 AM
what about ''fopen'' and ''fwrite'' ? we can't use them to open and write into a file ?
Where would such a file go, and what code do you have to support that operation? This is embedded, unless you've implemented some file system or OS it's not happening.You could output data via a serial port, or the SWV (View -> Serial Windows -> Debug (printf) Viewer) on the PB3 pin with SB10 bridged.2014-01-30 8:39 AM
''unless you've implemented some file system''
How can i implement file system ? it will be great. ''You could output data via a serial port'': yes i have tried to do that but no success, the communication works but when i send or receive data, i get wrong values so i dropped. Ideally, i want to store my two arrays into a file and then plot them with excel for example.2014-01-30 10:59 AM
Not sure why you have a problem with serial. Remember the STM32 uses CMOS levels, and won't connect directly to RS232 devices. You might want to look at USB-To-CMOS Serial type devices (FTDI, SiLabs, Prolific, etc)
File systems, on an STM32F3-Discovery you'd had to add an SD card socket/interface, add code to support that, and then add a file system like FatFsIf serial is a challenge, consider using the SWVhttp://www.keil.com/download/files/swv_on_cortex-m3.pdf
http://www.keil.com/download/files/labst.pdf
It works on the ST-LINK used on the STM32F3-DISCO board, you just need to bridge SB10 on the back to get the pin connectivity2014-02-03 9:26 AM
Hi again,
Thanks you clive1 for your help, i appreciate it.I use the SWV it works fine for simple data like printf(''hello word'').But when i want to print my two float arrays, i can't get all my data,my arrays are both 1024 samples, it jumps some value and i don't know why, for example it shows some thing like this:k=0 MES_1: -0.483102 MES_2: 0.347957 k=1 MES_1: -0.585388 MES_2: -0.821821 k=2 MES_1: -0.585826 MES_2: -0.821255 k=3 MES_1: -0.586605 MES_2: -0.819777 k=4 MES_1: -0.586402 MES_2: -0.819633 k=5 MES_1: -0.586548 MES_2: -0.821310 k=6 MES_1: -0.586817 MES_2: -0.821821 k=7 MES_1: -0.586755 MES_2: -0.821742 k=8 MES_1: -0.588197 MES_2: -0.819091 k=9 MES_1: -0.588505 MES_2: -0.818651 k=10 MES_1: -0.588773 MES_2: -0.817754 k=11 MES_1: -0.589459 MES_2: -0.823334 k=12 MES_1: -0.589924 MES_2: -0.818838 k=13 MES_1: -0.592064 MES_2: -0.820421 k=14 MES_1: -0.590832 MES_2: -0.817722 k=15 MES_1: -0.591669 MES_2: -0.816614 k=16 MES_1: -0.592894 MES_2: -0.816938 k=17 MES_1: -0.594940 MES_2: -0.815876 k=18 MES_1: -0.595303 MES_2: -0.814116 k=19 MES_1: -0.596574 MES_2: -0.814893 k=20 MES_1: -0.597424 MES_2: -0.814350 k=21 MES_1: -0.598700 MES_2: -0.813246 k=22 MES_1: -0.599896 MES_2: -0.812544 k=23 MES_1: -0.601454 MES_2: -0.813172 k=24 MES_1: -0.602724 MES_2: -0.810391 k=25 MES_1: -0.602640 MES_2: -0.811990 k=26 MES_1: -0.604783 MES_2: -0.810818 k=27 MES_1: -0.605809 MES_2: -0.808267 k=28 MES_1: -0.608684 MES_2: -0.808539 k=29 MES_1: -0.609863 MES_2: -0.806906 k=30 MES_1: -0.609863 MES_2: -0.805966 k=31 MES_1: -0.611337 MES_2: -0.807800 k=32 MES_1: -0.614956 MES_2: -0.803744 k=33 MES_1: -0.615910 MES_2: -0.802969 k=34 MES_1: -0.616941 MES_2: -0.804142 k=35 MES_1: -0.619237 MES_2: -0.801086 k=36 MES_1: -0.620757 MES_2: -0.799753 k=37 MES_1: -0.625475 MES_2: -0.802851 k=38 MES_1: -0.624527 MES_2: -0.798632 k=39 MES_1: -0.626367 MES_2: -0.795911 k=40 MES_1: MES_1: -0.521140 MES_2: 0.329964 k=233 MES_1: -0.510823 MES_2: 0.336236 k=234 MES_1: -0.503895 MES_2: 0.334139 k=235 MES_1: -0.492707 MES_2: 0.340790 k=236 MES_1: -0.480857 MES_2: 0.345976 k=237 MES_1: -0.470579 MES_2: 0.351589 k=238 MES_1: -0.461573 MES_2: 0.355391 k=239 MES_1: -0.450505 MES_2: 0.356636 k=240 MES_1: -0.441443 MES_2: 0.350977 k=241 MES_1: -0.430641 MES_2: 0.366206 k=242 MES_1: -0.425337 MES_2: 0.352911 k=243 MES_1: -0.411351 MES_2: 0.367043 k=244 40 MES_1: 0.321546 MES_2: -0.211932 .................................................. Do you have an idea what would be the problem ? i miss some configuration of the Trace ?Thanks in advance2014-02-03 9:29 AM
2014-02-03 9:36 AM
The SWV implementation has a finite buffer in the ST-LINK (J-LINK not much better), you might want to stop periodically. Serial is better for this because you can use flow-control.
If you copy (or have) your memory buffers in a known location like 0x20003000 you can SAVE that buffer. SAVE might also recognize symbols, although I've not used it in that fashion.2014-02-03 1:43 PM
And then how can i convert the Hex to float? do you know a software tool that can do this please ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.