STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CRC 8-bits on STMF4xx

Posted on February 04, 2014 at 12:45Hi,I want to calculate CRC with hardware CRC but polynomial on the register is work on 32 bits.Can possible to calculate CRC 8-bits with hardware in the MCU? And how?Or I have to use sw crc.Thank everyone.

suppakit by Associate II
  • 1428 Views
  • 3 replies
  • 0 kudos

12bit DAC performance

Posted on February 04, 2014 at 15:28Hi there,In my application I need precise control of applied voltage. I use 12bit DAC with 2.5V reference. The mcu is stm32f107I was going to do error budget analysis but was confused by the datasheet. It gives +/...

oleg by Associate
  • 1313 Views
  • 3 replies
  • 0 kudos

USB CDC Host example

Posted on December 08, 2011 at 08:50Hi ! I need to implement an USB CDC Host on STM32F4 Controller. Has anyone an example, or some hints how to do that ? I only found examples for CDC Device applications. regards Marc

doebber2 by Associate II
  • 6946 Views
  • 14 replies
  • 0 kudos

PWM Feedback STM32F103ZE

Posted on February 03, 2014 at 08:00The original post was too long to process during our migration. Please click on the attachment to read the original post.

liviana by Associate II
  • 3947 Views
  • 6 replies
  • 0 kudos

SAVE MEMORY CONTENTS TO A FILE for STM32F3

Posted on January 29, 2014 at 17:00Hi all; I'm working with the discoveryF3  board, i'm using the ST-Link debugger. I want to save two float arrays into a file when debugging. My IDE is µVision4. I found that the command ''save'' can do that  but ...

ADC1 STM32F0

Posted on January 30, 2014 at 03:56 Hi all, I just started working with STM32F0. I want to try ADC1 in this board but I find some trouble. I want to turn on the LED (PC8 and PC9) by using ADC asbenchmark, so when ADC1 reach 2000 bit or7D0...

sky_brake by Associate II
  • 2573 Views
  • 5 replies
  • 0 kudos

strange spi signal problem

Posted on February 28, 2013 at 14:40Hello everyone, We are using STM32F215VGT on our project. When we send data over SPI from STM32F2, clock and data signals are not square wave. i attached clock signal. On our board, there is TXB0106 between STM32...

0690X00000602kpQAA.jpg 0690X00000602nxQAA.jpg
ckaya by Associate II
  • 3455 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.