2016-10-12 3:41 PM
Hello,
Will the following generate a 50 Hz pulse?(Since htim3.Init.Period = 19999 which I think equates to ~20ms) htim3.Instance = TIM3; htim3.Init.Prescaler = 83; htim3.Init.CounterMode = TIM_COUNTERMODE_UP; htim3.Init.Period = 19999; htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; if (HAL_TIM_Base_Init(&htim3) != HAL_OK) { Error_Handler(); }Thanks,Sel2016-10-12 6:34 PM
I have an update.
On the scope, I see 3.7 Hz. I would appreciate any feedback on how TIM works (and how to achieve 50 Hz)Thanks,Sel2016-10-12 7:00 PM
Looks like I can play with htim3.Init.Prescalar, Period, and sConifigOC.Pulse to manipulate the waveform properties (Frequency and Duty cycle).
At this point, I am just turning the knobs without a clear understanding all the dependencies and how to calculate the outcome. I tried a setting with Prescaler = 16, Period = 7499, and Pulse=800 and was able to see a 50 Hz waveform with close to 10% duty cycle. But, it appears it is not stable and the waveform keeps collapsing (and I have to reset the board).2016-10-13 2:11 AM
Hi Sel,
To let other users in Forum helping you , try to share details abbout your request: Which device you are using ?Which board ?Wich library you use ? which version ?you shoud share code or part of it (as TIM configuration)-Hannibal-2016-10-13 2:18 PM
Hi Hannibal,
Thanks. I am trying to vary PWM width (duty cycle) as shown in the while loop below. I am using STM32F407VGTx (on the STM32F4 Discovery board). Here is the version information:@file stm32f4xx_hal_tim.h * @author MCD Application Team * @version V1.5.2 * @date 22-September-2016 * @brief Header file of TIM HAL module.Here is the code I have in main.c:int main(void){ /* MCU Configuration----------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_TIM3_Init(); HAL_TIM_Base_Start(&htim3); HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_2); MX_USART2_UART_Init(); //Trying to step through various duty-cycle values while (1) { HAL_Delay(1000); sConfigOC.Pulse = 100; HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2) HAL_Delay(1000); sConfigOC.Pulse = 400; HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2) HAL_Delay(1000); sConfigOC.Pulse = 800; HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2) }}/* TIM3 init function */static void MX_TIM3_Init(void){ TIM_ClockConfigTypeDef sClockSourceConfig; TIM_MasterConfigTypeDef sMasterConfig; TIM_OC_InitTypeDef sConfigOC; htim3.Instance = TIM3; htim3.Init.Prescaler = 16; htim3.Init.CounterMode = TIM_COUNTERMODE_UP; htim3.Init.Period = 7499; htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; if (HAL_TIM_Base_Init(&htim3) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_Init(&htim3) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK) { Error_Handler(); } sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = 800; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2) != HAL_OK) { Error_Handler(); } HAL_TIM_MspPostInit(&htim3);}2016-10-17 10:29 AM
Hi Sel,
If you want to modify the PWM on the fly, you ought to do thatin interruption. In case, you want that in a programmable delay, you should use the systick interruption or a timer channel interrupt. In case , you want to control the PWM signal and after a certain number of pulses you dou your modification, you ought to control it using another timer input.-Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.