2016-05-12 8:25 AM
Hi.
I have a problem withresistive TP.
I use STMPE811.
I use my custom board with connection of the stmpe811 similar to the stm32f429discovery board, as well as the drivers from the board demonstration software.
I cannot get correctvalues of x and y.
To isolate the problem I take the values of x and y immediately after this function –stmpe811_TS_GetXY(...) and print them to the screen. The values are quite unstable. For example when I push in some part of the screen I receive something like this x = 1230, y = 3457. Holding the finger in the same spot the values of x and y change slightly (+-50) but once in 2-3 seconds those values are something absolutely different like x= 60, y = 6354234.
Another problem is when I move finger along the x axis the value of y also changes by several times (but it should stay the same as I don't change y position).
I tried to change touch detect delay, average control samples – the problem had notchanged.
Just for reference hereare the values of the corners:
left upper x = 2720, y = 3500
left lower x = 1900, y = 4300
right upper x = 4020, y = 3600
right lower x = 530, y = 52014
middle of the screen x = 3670, y = 2180
As I mentioned the values are something absoultely different once per 2-3 seconds.
Is there something I can check?Thanks.
2016-05-16 12:46 AM
Still did not run the touch screeen.
Here is the function stmpe811_TS_GetXY.It reads data from the register STMPE811_REG_TSC_DATA_NON_INC (0xD7).However I did not find this register in the datasheet.I also checked revision number (ID_VER) and it is 0x03 (the datasheet mentions only 0x01 version).I checked the TP (actually two TPs) with voltmeter and it responses properly...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.