2016-05-15 7:05 PM
Hello all,
I want to configure LPTIM_1 for an external pulse count application (~10MHz signal). I request to know whether any highest frequency limit? For signals more than ~200KHz, its giving 0 count. Less than 200KHz seems ok. I've connected a square wave input (PB5 pin Nucleo) and configured as both LPTIM_1 external clock and external counter input (using Low Level Cube Library). I'm logging LPTIM_1 count value in every 5ms (LPTIM_2 interrupt) using UART and calculating the difference for exact count values. Am I missing anything in LPTIM_1 configuration? I request your kind suggestion. void Configure_LPTIMCounter1(void) { LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOB); LL_GPIO_SetPinMode(GPIOB, LL_GPIO_PIN_5, LL_GPIO_MODE_ALTERNATE); LL_GPIO_SetPinPull(GPIOB, LL_GPIO_PIN_5, LL_GPIO_PULL_DOWN); LL_GPIO_SetPinSpeed(GPIOB, LL_GPIO_PIN_5,LL_GPIO_SPEED_FREQ_VERY_HIGH); LL_GPIO_SetAFPin_0_7(GPIOB, LL_GPIO_PIN_5, LL_GPIO_AF_1); LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_LPTIM1); LL_LPTIM_SetClockSource(LPTIM1, LL_LPTIM_CLK_SOURCE_EXTERNAL); LL_LPTIM_SetCounterMode(LPTIM1, LL_LPTIM_COUNTER_MODE_EXTERNAL); LL_LPTIM_SetUpdateMode(LPTIM1, LL_LPTIM_UPDATE_MODE_IMMEDIATE); LL_LPTIM_Enable(LPTIM1); LL_LPTIM_SetAutoReload(LPTIM1, 0xFFFF); LL_LPTIM_StartCounter(LPTIM1, LL_LPTIM_OPERATING_MODE_CONTINUOUS); }2016-05-15 11:56 PM
There might be some gotcha in the setup. I'd try internal clock and external counter input (LPTIMx_CFGR.CKSEL = 0, LPTIMx_CFGR.COUNTMODE = 1); of course no filter no prescaler etc. Also, please post registers content to avoid any library involvement.
Nevertheless... I can find no relevant LPTIM data in the current rev4 'L476 datasheet, nor in the current rev4 'F745 datasheet. This very question has been asked at the ST seminar I attended last December, after having been told that as an asynchronous timer it would run up high regardless of the internal clock; and the support could not come up with definitive answer either. Sorry, but this is a shame, ST. A good place to come up with relevant information would be the promised renewed Technical Journal... JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.