2017-04-01 3:18 PM
It happens many times that I find a bug inside the Cube/HAL driver or even inside the comments and documents and I really want to report it, so they can FIX it, thus making a bug free environment to develop my/our applications, BUT the lack of a bug tracking system prevents me to report it.
Even though I see some users report bugs in the forum, but it feels like useless as nobody replys to them or they can't find out if their contribution into fixing bugs has been observed by ST employees.
So, my request is starting a bug reporting/tracking system. I think it's a win-win suggestion.
#bug #request2017-04-02 2:04 AM
I bet they have a bugtracking software in place internally, without access from 'outsiders' like here on this forum.
But let's see what the ST staff tells us ...
2017-04-02 6:10 AM
Maybe a git of the source files would make the loop back more reactive?
2017-04-02 2:07 PM
I would like to ask some of moderators forward this request to staffs if possible.
2017-04-02 2:52 PM
nice, so we can commit changes and request for a pull
2017-04-02 5:18 PM
+1 would be really nice and would probably save some time on ST's side, too
2017-04-03 2:30 AM
Hello,
I will raise your request internally.
All your comments and suggestions are welcome in order to improve our solutions.
Imen
2017-04-04 8:02 AM
There definitely needs to be change in release and test strategy, where bug tracking goes along with Regression Testing and Dog Fooding of the released code.
The embedded ecosystem needs solid, tested code, you need to apply the TEN YEAR commitment to the expectation for your code. Many applications aren't going to have easy opportunities to field upgrade and may be deployed for decades. It is incumbent on ST to do a better job with the code quality.
The bug tracking has been requested repeatedly, posting unformated/unfocused bug reports to the forum is not sufficient. There needs to be ownership. You have thousands of eyes on the code, you need to use them effectively.
2017-04-04 10:05 AM
>>
I bet they have a bugtracking software in place internally
Let's hope so, but there really doesn't seem to be a lot of rigour in the testing and critical review of the code.
2017-04-04 12:32 PM
The bug tracking has been requested repeatedly, posting unformated/unfocused bug reports to the forum is not sufficient. There needs to be ownership. You have thousands of eyes on the code, you need to use them effectively.
Linux, especially the kernel, are examples that this might work - on professional level, with professional results.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.