2017-01-11 9:22 AM
I have tried to reflash St-Link by J-Link. But has got an error: Timeout: ST-LINK/V2-1 did not enter DFU mode
Now ST-Link is not detected.
Is there any way to reflash st-link on the board by other board or so?
2017-01-11 9:37 AM
No, no other firmware or method is provided to recover the ST-LINK
I've seen a similar error, which is generally non-fatal when upgrading the ST-LINK via the utilities, and it is in the wrong state. Usually recover that by resetting the board, or unplugging and plugging back in, and not using it in Keil, IAR, etc.
2017-01-11 9:57 AM
Two methods:
- Ask you FAE about the STLINK and it's firmware
- Get access to the F103 Chip via Bootloader or SWD and flash the firmware from STLinkV2.J16.S4.zip found in the GrayNet (some russian site).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.