STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Receive works on STM32F103 and doesn't work on STM32F427

Posted on January 10, 2017 at 18:10Hello,For the past month I have been developing a device that has multiple features on an STM32F103ZG, with the intentions of basically replacing the chip and migrating the code with an STM32F427ZI when I was close...

Popcorn by Associate II
  • 4375 Views
  • 6 replies
  • 0 kudos

Resolved! SPI interrupt problem (repetition)

Posted on January 11, 2017 at 21:22Hi,Here is my program#include <stdio.h>#include <string.h>#include 'stm32f10x_gpio.h'#include 'stm32f10x_rcc.h'#include 'stm32f10x_usart.h'#include 'stm32f10x_spi.h'#define SPI_FLASH           SPI3#define SPI_CLK  ...

parisa by Senior
  • 987 Views
  • 1 replies
  • 0 kudos

HAL_NVIC_EnableIRQ while thread executing

Posted on January 11, 2017 at 18:58Hi all, I'm using STM32L4 MCU and FreeRTOS V8. I have implemented thread that execute normaly, During this thread, I have to initialize HAL interrupt (by executing  HAL_NVIC_EnableIRQ(EXTI9_5_IRQn); ) Unfortunately...

Reflash ST-Link on discovery board

Posted on January 11, 2017 at 18:22I have tried to reflash St-Link by J-Link. But has got an error: Timeout: ST-LINK/V2-1 did not enter DFU modeNow ST-Link is not detected.Is there any way to reflash st-link on the board by other board or so?

kozlovdmn by Associate II
  • 1396 Views
  • 2 replies
  • 0 kudos

STM32 chips with native modbus support

Posted on December 30, 2016 at 22:20Hello there,Is there any list of STM32 devices with native ModBus support? I am trying to find a proper mcu and I have to open each datasheet by hand and ctrl+F for modbus. There has to be a better way. So far I h...

TIM5 counter

Posted on September 02, 2016 at 12:41Hi all,I want to count pulses from an input, using TIM5 channel 3, I have tried with channel 1 and it is working but I cannot make it works in channel 3 , can someone let me know what can be wrong.This is the cod...

jampino by Associate III
  • 2305 Views
  • 8 replies
  • 0 kudos

epoch time

Posted on January 11, 2017 at 14:59I'm using a NUCLEO-144 with an STM32F412ZG MCU. I'm having issues with the time() function. If I load my application via the debugger, the call to time() gives me the desired result. If I run my application normall...

Joe M. by Associate
  • 933 Views
  • 1 replies
  • 0 kudos

EEprom faliur

Posted on January 11, 2017 at 06:22I have write a string on multiple address of eeprom but when i read it later it show FF on some places between the data but sometime it reads every thing fine. I am using this library http://www.electroons.com/blog...

daynial by Associate II
  • 675 Views
  • 1 replies
  • 0 kudos

Cannot locate core_cmInstr.h

Posted on January 05, 2017 at 03:07Hello, i am new in linux, i am using the STM32 Crypto lib and try to work on the RSA part,i am using linux command build.I get the error ofcore_cm3.h:136:95: fatal error: core_cmInstr.h: No such file or directory m...

FLast.11 by Associate III
  • 2800 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.