2015-09-10 1:41 AM
Im using the stm32f407vg discovery board, and coocox is my ide.
Im trying to use Random number generator (RNG) to generate true random number. Please see code attached. When i run it, it get stuck in ''while(RNG_GetFlagStatus(RNG_FLAG_DRDY)== RESET)'' loop, ie number isnt ready to be read. Am I missing the setup of some register. #stm32f407-random-number-generate2015-09-10 3:24 AM
RNG has clock from PLL48CLK, so you have to have PLL running and PLLQ set adequately.
RNG is one of the things which can be debugged by directly writing/reading registers in the debugger. JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.