2013-05-07 6:29 AM
We're using RTC as a timer to wakeup STM32F103 from stop mode frequently, I'm quite confused on the descriptions in RM0008
1. what's the difference between RTC_IRQHandler and RTCAlarm_IRQHandler? If an alarm comes, both irq called? Is there a EXTI17_IRQHanlder?2. do I must clear all of EXTI_Line17, PWR_FLAG_WU, RTC_IT_ALR in some irq handler? what's the actual physical connection between the components that these registers reside on (plz help to explain based on Figure 179 in RM0008)?Thanks a lot! #rtc #stm32f1We’re moving the ST Community to a new platform to give you a better and more reliable community experience.