STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Tx-Rx problem with USART in STM32L- Discovery !

Posted on April 25, 2012 at 17:11This is my code for Transmission :void USART3_tx(void){ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure;   /* Enable GPIOB and USART3 clock */  RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART...

ChibiOS mp3 player

Posted on May 08, 2013 at 05:53Has anyone ever tried using the mp3 player on the ChibiOS website? I downloaded the project file, uploaded the prebuilt binary to my board, but cannot get any sound out of my board. I got the mp3 files in the root dire...

TIM1 update interrupt problem

Posted on May 07, 2013 at 15:16I initialized two timers (TIM1 and TIM3) on STM32F100R6 the same way to give an update interrupt. Now it seems both timers run at the same speed, but the update interrupt on TIM1 occurs not that often like TIM3 does. B...

keckardt by Associate
  • 1220 Views
  • 1 replies
  • 0 kudos

MEMS: paralleling sensors to reduce noise?

Posted on May 07, 2013 at 15:56Hi, I've heard there is a way to reduce noise (and increase performances) of MEMS sensors. Let's suppose I'm using MEMS single axis accelerometer: Noise = 32 mg RMS value in band 0-100HZ Output (digital) = 1024 counts ...

mbertoni by Associate II
  • 1120 Views
  • 1 replies
  • 0 kudos

Question about the RTC of STM32F103

Posted on May 07, 2013 at 15:29We're using RTC as a timer to wakeup STM32F103 from stop mode frequently, I'm quite confused on the descriptions in RM00081. what's the difference between RTC_IRQHandler and RTCAlarm_IRQHandler? If an alarm comes, both...

qinghui by Associate
  • 922 Views
  • 0 replies
  • 0 kudos

need a working code for CAN protocol by stm32f3 discovery kit

Posted on May 07, 2013 at 14:01hello ,i check STM32F3-Discovery_FW_V1.1.0 folder where all example for stm32f3 discovery is given . but here is no project for CAN protocol . please send me code example or link from where i can get the working code ....

raj2 by Associate II
  • 1150 Views
  • 2 replies
  • 0 kudos

AN3990 firmware

Posted on May 03, 2013 at 18:25Hi guys,I cannot find source code for AN3990; there is someone that can kindly give me the right link? Thank youMarco #an3990

STM32F400 and CS42L52 audio codec

Posted on April 16, 2013 at 13:09Hi! I have a big problem and need a lot of help. First of all I will try to explain the global situation and after that I will ask you for some questions. I am working in a project. I have to make a full-duplex audio...

rafael23 by Associate II
  • 6270 Views
  • 15 replies
  • 0 kudos

RS485 modbus Communication

Posted on March 25, 2013 at 13:01i am using the stm32f107rc  controller for rs485 communication. i am trying to transmit a set of data through usart1 from the controller, but some byte of data are missing at the destination so pls let known where i ...

aru by Associate II
  • 3825 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.