2020-12-03 5:19 PM
I have a straightforward question regarding the DWT counter. I am using the DWT->CYCCNT counter to count clock cycle differences in the STM32L431CC, and I noticed that CYCCNT is 32-bits wide. If I were to use HSI16 as my internal clock source, the CYCCNT would still go up to the maximum value of a uint32_t which is 4294967295, and not 16000000 based on my HSI16 clock source right?
Thanks!
timestamp_1 = DWT->CYCCNT;
DoSomeTask();
timestamp_2 = DWT->CYCCNT;
if(timestamp_2 < timestamp_1)
{
/* I originally filled 16000000 instead of MAX_INT here */
timedifference = timestamp_2 + MAX_INT - timestamp_1;
}
else
{
timedifference = timestamp_2 - timestamp_1;
}
Solved! Go to Solution.
2020-12-03 5:37 PM
Correct.
Also, because it's 32-bits, you don't need to do any fancy logic based on if the new value is less than the old one. The overflow will get this correct.
uint32_t timestamp_1 = DWT->CYCCNT;
DoSomeTask();
uint32_t timestamp_2 = DWT->CYCCNT;
uint32_t duration_ticks = timestamp_2 - timestamp_1;Your code as written will be off by 1 in the case that timestamp_2 < timestamp_1.
2020-12-03 5:37 PM
Correct.
Also, because it's 32-bits, you don't need to do any fancy logic based on if the new value is less than the old one. The overflow will get this correct.
uint32_t timestamp_1 = DWT->CYCCNT;
DoSomeTask();
uint32_t timestamp_2 = DWT->CYCCNT;
uint32_t duration_ticks = timestamp_2 - timestamp_1;Your code as written will be off by 1 in the case that timestamp_2 < timestamp_1.
2020-12-03 5:54 PM
Thanks for the answer TDK! I was not aware of that last part though, thanks for adding that to your answer too.
2020-12-03 10:38 PM
I have been thinking about this, and I am still curious if this would work for clock cycle counts at the higher extreme end. If, for example:
timestamp_1 = 0xFFFFFFFF;
timestamp_2 = 0x00000001;
// duration_ticks = timestamp_2 - timestamp_1 = 0xFFFFFFFE;yet, in the example above, it would only take 2 clock cycles to go from timestamp_1 to timestamp_2. If timestamp_1 + 2 clockcycles, it would be:
// timestamp_2 + 2 = 0xFFFFFFFF + 0x2 = 0x1 0000 0001
/* Since only the last 32-bits are included, that would mean DWT->CYCCNT would still hold
the value 0x00000001 wouldn't it?
*/I would still need the logic wouldn't I (which would include adding timestamp_2 by the MAX_UINT32 and then subtract that summation with timestamp_1? Or is my understanding about the 32-bit DWT->CYCCNT counter incorrect?
Thanks!
2020-12-04 7:09 AM
> timestamp_1 = 0xFFFFFFFF;
> timestamp_2 = 0x00000001;
> // duration_ticks = timestamp_2 - timestamp_1 = 0xFFFFFFFE;
This is not what duration_ticks would equal. It would equal 2.
> I would still need the logic wouldn't I
No, it will still give you the correct answer. Try it:
https://onlinegdb.com/ry_rlCPoP
In mathematical terms, results are calculated modulo 2^32.
2020-12-04 1:27 PM
Hi TDK, thanks for the example and explanation! I think I understand what you are talking about now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.