2014-10-15 12:26 AM
Hi,
I have working code on STM32F407 discovery board and would like to port it to discovery board based on STM32F429. If I set GPIO_Mode_IN on STM32F429 I can see nice shaped signals from encoder on input pins PA1 and PA5. When I set GPIO_Mode_AF pins seems to be driven low from STM32F429 side. AF is set to TIM2 with: GPIO_PinAFConfig(GPIOA,GPIO_Pin_5,GPIO_AF_TIM2); GPIO_PinAFConfig(GPIOA,GPIO_Pin_1,GPIO_AF_TIM2); Code for timer setting is same for both STM32F407 and STM32F429:TIM_TimeBaseStructure.TIM_Prescaler = 0x00;
TIM_TimeBaseStructure.TIM_Period = 65536; //max resolution
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV4;//divide by clock by one
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;// count up
TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
TIM_EncoderInterfaceConfig(TIM2, TIM_EncoderMode_TI12, TIM_ICPolarity_Falling, TIM_ICPolarity_Rising);
TIM_ICStructInit(&TIM_ICInitStructure);
TIM_ICInitStructure.TIM_ICFilter = 0;//ICx_FILTER;
TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; TIM_ICInit(TIM2, &TIM_ICInitStructure);TIM2->CNT = 0;
TIM_Cmd(TIM2, ENABLE);//enable encoder Any ideas what can be wrong or differences between 32F407 and 32F429 that can trigger this problem? Regards, Aleksandar #quadrature-encoder-stm32f4292014-10-15 1:31 AM
Hi Aleksander,
There are 2 axes for checks:1- Hardware side: review differences between both boards that may impact your application.2- Software side: if you are enabling alternate functions on pins PA1 & PA5 after enabling TIM2 clock please try to do the inverse & check again. I am interested to know results.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-10-15 3:29 AM
GPIO_PinAFConfig(GPIOA,GPIO_PinSource5,GPIO_AF_TIM2);
GPIO_PinAFConfig(GPIOA,GPIO_PinSource1,GPIO_AF_TIM2);2014-10-15 3:58 AM
Thanks!
I made mistake during porting. After all both macros are really similar. BR, AleksandarWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.