2024-05-08 1:42 AM - edited 2024-05-08 1:45 AM
Hi,
I've been trying to have a output quadrature and I somehow managed to do it with this code.
void TIM3_Configuration_positive_quadrature(void)
{
TIM_OCInitTypeDef TIM_OCInitStructure;
int Period;
Period = 1000 / 1; // 1 Hz - 1 second on, 1 second off duty
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_Pulse = (Period * 1) / 4; // CH3 at 25%
TIM_OC3Init(TIM3, &TIM_OCInitStructure);
TIM_OCInitStructure.TIM_Pulse = (Period * 3) / 4; // CH4 at 75%, ie half cycle later
TIM_OC4Init(TIM3, &TIM_OCInitStructure);
}
I set the frequency to 1500 Hz and run the quadrature function above but when I do it I see the quadrature on the oscilloscope but the frequency changes value continuosly to random values (for example 340, 420, 383, 540 Hz and so on) and can't understand what causes it.
Any help is appreciated :)
2024-05-08 4:30 AM
Look for fundamental problems in you setup. I doubt you set the frequency you expect. How did you measure? With a scope? Did you perhaps have aliasing?
2024-05-08 4:39 AM
I measure it with a scope and also have a software that displays the frequency set.
I double checked and I set the correct frequency but as soon as I call the function of the quadrature the frequency starts going crazy.
No aliasing.
2024-05-08 7:03 AM - edited 2024-05-08 8:06 AM
On the oscilloscope I see half of the frequency I set, after calling the quadrature function.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.